Post Go back to editing

ver 2.1.0 installation

Thread Summary

The user inquired if the USB driver installation for ADALM2000 and Pluto SDR is necessary when using Scopy v2.1.0 on Windows 11. The final answer confirms that the USB drivers are required for the system to detect the devices, but if already installed, they do not need to be reinstalled from the Scopy setup. The user's ADALM2000 is functioning correctly.
AI Generated Content
Category: Software
Product Number: ADALM2000

Hello

In order to use ADALM2000, I had just download below for my Win11 PC.  

Scopy-v2.1.0-Windows-setup

I think installation of  usb driver (Pluto SDR and M2k) (**)  was not necessary for Scopy ver 2.1.0 , because   all components   necessary may be included .

(**)

Windows Drivers [Analog Devices Wiki]

Is my understanding wrong?

I am using ADALM2000 and its OK.

Could you please correct procedure for D/L scopy latest version to Win 11 PC?

Best Regards

Edit Notes

typo was fixed
[編集者:shiba183、編集時刻: 5 Nov 2025 日 5:03 AM 時 (GMT -5)]
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.