Post Go back to editing

Regarding FMCW_Velocity_RADAR_Waterfall.py Python Script Example

Thread Summary

The user encountered issues with velocity measurements using the FMCW_Velocity_RADAR_Waterfall.py script on a Phaser board, showing only static at 0 value. The support engineer confirmed the script was incomplete and recommended using Range_Doppler_Plot.py instead. The user resolved the issue by reducing the max_range variable to 10 meters, allowing for accurate indoor testing with a moving target.
AI Generated Content
Category: Software
Product Number: CN0566

Very Good Day,

I'm in the middle of testing my Phaser board. When I run a Python script (FMCW_Velocity_RADAR_Waterfall.py) by Jon Kraft, the velocity measurements was not coming up. The graph shows only static at 0 value. Do any one experienced the same during testing it?

Parents
  • Please provide information about your setup, exactly what you are seeing, and any error messages.  Also ensure that you have followed the complete getting started guide here: https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0566/quickstart

    And have connected the included ribbon cable between Pluto and the Phaser board.  It is helpful if you can provide some pictures of your setup as well.  Thanks!

  • Thanks for your quick response Jon. I really appreciated it.

    For your info, I already test the board for CW radar with some additional features and it works. It measured velocity with graph and PPI for visualization. Below are the video:

    And I already test FMCW radar using an example on the local phaser folder (Raspberry PI) and it also works. Below are my setup pictures:

    I already connected the ribbon cable, as seen from the picture. But the problem is with FMCW_Velocity_RADAR_Waterfall.py from your github page, it is not shown any velocity measurement on the graph during target movement. But FFT spectrum clearly shows the beat frequency movement as shown on below pictures:

    Right now I tried to do my own algorithm to compute the velocity for FMCW radar. I hope you can assist me regarding the matters.

    Thank you...

Reply
  • Thanks for your quick response Jon. I really appreciated it.

    For your info, I already test the board for CW radar with some additional features and it works. It measured velocity with graph and PPI for visualization. Below are the video:

    And I already test FMCW radar using an example on the local phaser folder (Raspberry PI) and it also works. Below are my setup pictures:

    I already connected the ribbon cable, as seen from the picture. But the problem is with FMCW_Velocity_RADAR_Waterfall.py from your github page, it is not shown any velocity measurement on the graph during target movement. But FFT spectrum clearly shows the beat frequency movement as shown on below pictures:

    Right now I tried to do my own algorithm to compute the velocity for FMCW radar. I hope you can assist me regarding the matters.

    Thank you...

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.