Post Go back to editing

SCOPY spectrum measurement start frequency lower and narrower BW for 1/f noise

Thread Summary

The user asked about measuring 1/f noise of an op-amp from 0.1 Hz to 1 kHz using SCOPY, but SCOPY limits the start frequency to 1 Hz and has a wide resolution bandwidth (RBW). The final answer suggests capturing data at the lowest possible sampling rate and applying additional decimation in MATLAB or another tool to achieve the desired RBW. The user confirmed that SCOPY cannot meet the desired settings and the thread was closed due to inactivity.
AI Generated Content
Category: Software
Product Number: SCOPY
Software Version: V2.1.0-rc2

Hi,

I would like to measure OP amp 1/f noise and its desired range is 0.1 Hz to 1 kHz.

I set SCOPY to log frequency mode and tried to lower its start frequency. SCOPY limits its frequency up to 1Hz and its bin width (RBW) is too wide for the desired measurement.

Is it possible making SCOPY spectrum measurement frequency lower (like 0.1Hz or 0.01Hz if possible) and spectrum bin width (RBW) much more (like 0.01Hz)?

Attachment is a capture what I could (but not fit my desired setting)

PDF 

Please advise.

Regards,

Satoru