Post Go back to editing

CN0566 Real-time data processing and beamforming control to track targets

Thread Summary

The user inquires about real-time beam control for human or drone tracking using the CN0566 phased array radar, facing delays due to processing times. The final answer suggests using GNURadio with a remote host computer instead of a Raspberry Pi to handle the data processing, noting the USB connection as a bandwidth limitation for the PlutoSDR. The user can also disconnect the PlutoSDR and use their own SDR by carefully managing the U.FL RX connectors on the phaser board.
AI Generated Content
Category: Hardware
Product Number: CN0566

Dear Professor,

Hello. I have encountered the following issue using the CN0566 phased array radar: when I track a human or a drone, I want to control the beam direction using the latest data instead of processing after data acquisition. However, the processing time inevitably takes a long time. In the example code, the sum-difference beam tracking is in the time domain, but when detecting a human or a drone, it is necessary to perform a range FFT, and if needed, also a range-Doppler FFT. Therefore, in practice, only data from a long time ago can be processed each time, and the angle data after processing, when used for current beamforming, is already outdated. Given all this, does your hardware setup make it impossible to achieve real-time beam control for human or drone tracking tasks and only allow observation via range-Doppler?

Edit Notes

Corrected a grammatical error
[edited by: HelloQiLin at 3:47 AM (GMT -4) on 18 Oct 2025]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.