Post Go back to editing

Scopy v2.1.0 Software Broken for MacOS 15.6.1 (Sequoia)

Thread Summary

The user encountered a crash issue with Scopy software on macOS 15 when attempting to connect to the ADALM2000. The problem was resolved by resetting Scopy preferences. A crash log was provided, showing an abort trap and issues with the `libm2k` and `libusb` libraries during the connection process.
AI Generated Content
Category: Software
Product Number: ADALM2000
Software Version: 2.1.0

I am having issue getting the Scopy software to run on MacOS 15. The software installs fine, and the first time I installed and launched it, I was able to use my ADALM2000 without issue. As soon as I relaunched the program, it continues to crash as soon as I tell the software to connect to the ADALM2000. I have tested this with multiple ADALM2000 units and have verified that this is software and not hardware related. I have also tried reinstalling the software multiple times without any luck. Any help would be appreciated, but this seems to be an issue with the software release itself.

Parents Reply Children
  • I am not able to reproduce this issue, could you tell me the exact steps you are taking to reproduce the bug? 

    Thanks!

  • I was able to reproduce the bug by using the ADALM device with the Scopy software. I then closed out of the Scopy software without disconnecting from the ADALM, the ADALM also had modules enabled (oscilloscope and function generator). Then on subsequent launches when connecting to the ADALM again, this is where the crash is occurring. I wasn't able to consistently reproduce it, but it has something to do with this process. Hope this helps you reproduce the bug on your end. 

  • I was still not able to reproduce the issue. Even when trying on multiple devices.
    Like my colleague said it would help if you could attach the Scopy.ini and Preferences.ini files when you are getting the crash so we can investigate. They are found here:

    • Windows: C:\Users\<your_username>\AppData\Roaming\ADI Sometimes this is a hidden directory, and you unhide it.
    • Linux: /home/<your_username>/.config/ADI
    • Mac: /Users/<your_username>/.config/analog.com

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.