Post Go back to editing

ADALM2000 LAbVIEW Errors

Thread Summary

The user encountered an error (1097) when running an ADALM2000 example in LabVIEW, despite installing the libm2k-0.9.0 and libm2k LabVIEW v1.0.0.1 packages and updating the firmware to v0.33. The final solution suggested trying the libm2k LabVIEW v1.0.0.2 package.
AI Generated Content
Category: Software
Product Number: ADALM2000
Software Version: LabVIEW 2020

Hello I am needing to use the ADALM2000 on labVIEW for a project.

Following the guide found wiki.analog.com/.../labview I have:  

-Downloaded and installed libm2k-0.9.0-Windows-setup.exe on https://github.com/analogdevicesinc/libm2k/releases/tag/v0.9.0 and ticked the “Install wrapper for LabVIEW bindings” box.

-Downloaded libm2k LabVIEW v1.0.0.1 from github.com/.../releases and added the package to the VI package manager.

-Downloaded the 'source code' file and ensured libm2k_lv.dll is on the system path.  

When attempting to run an example from the sample library I run into the following error message:

"Error 1097 occurred at Call Library Function Node in Power Supply Enable All Out.vi->Example Power Supply.vi Possible reason(s): LabVIEW: (Hex 0x449) An exception occurred within the external code called by a Call Library Function Node. The exception might have corrupted the LabVIEW memory. Save any work to a new location and restart LabVIEW."

Is there any method to solve this issue?  

Best regards, Liam  

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.