Post Go back to editing

I'm not on 192.168.2.*

Category: Software

My home network is 192.168.178.* and I can't access my Pluto via ssh with USB under 192.168.2.1. I'm running with Linux. My routers adress is  192.168.178.1. I tried different settings. My actual config.txt is:

# Analog Devices PlutoSDR Rev.C (Z7010-AD9363)
# Device Configuration File
# 1. Open with an Editor
# 2. Edit this file
# 3. Save this file on the device USB drive
# 4. Eject the device USB Drive
# Doc: wiki.analog.com/.../customizing

[NETWORK]
hostname = pluto
ipaddr = 192.168.178.190
ipaddr_host = 192.168.178.1
netmask = 255.255.255.0

[WLAN]
ssid_wlan = MyWLAN
pwd_wlan = xxxxxxxxxx
ipaddr_wlan = 192.168.178.190

[USB_ETHERNET]
ipaddr_eth = 192.168.178.190
netmask_eth = 255.255.255.0

[SYSTEM]
xo_correction =
udc_handle_suspend = 0
# USB Communication Device Class Compatibility Mode [rndis|ncm|ecm]
usb_ethernet_mode = ncm

[ACTIONS]
diagnostic_report = 0
dfu = 0
reset = 0
calibrate = 0

Thanks for your help in advance!

Edit Notes

added router adress
[edited by: gatonero at 2:32 PM (GMT -4) on 9 May 2025]
Parents
  • Hello, 

    Can you check if the drivers are installed there are detailed steps on how to do this here 

  • Everything is installed.

    iio_info -s  
    Available contexts:
           0: (mt7921_phy0,hidpp_battery_0,acpitz,hidpp_battery_1,coretemp,nvme on Default string) [local:]
           1: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=10447318ac0f0011060036002b8c172932 [usb:3.9.5]

  • Seems that there is the same result:

    iio_info -s                                                                                                                    Heavy check mark  
    Available contexts:
           0: (mt7921_phy0,hidpp_battery_0,acpitz,hidpp_battery_1,coretemp,nvme on Default string) [local:]
           1: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=10447318ac0f0011060036002b8c172932 [usb:3.9.5]

    But there are three new files: 

    1. ipaddr-usb0, which is empty
    2. status, content: "here 1:"
    3. SUCCESS_ENV_UPDATE, which is empty also

    These files disapear after a reboot.

  • can you run iio_info -u ip:192.168.178.2 
    To check if we are able to see the context like this ? 

  • iio_info -u ip:192.168.178.2                                                                                                   Heavy check mark  
    Unable to create IIO context ip:192.168.178.2: Connection refused (111)

  • can you try to make a firmware update following the instructions here and then try again to configure your custom ip config ? 

  • On 192.168.178.2 there was a repeater. The repeater is now offline and I removes it's settings in my router. Now:

    iio_info -u ip:192.168.178.2                                                                                          1 ✘  3s   
    Unable to create IIO context ip:192.168.178.2: No route to host (113)

  • For now try to update the firmware.
    After the update try to run iio_info -u ip:192.168.2.1 with no other changes made. 

  • If this does not work use the config file bellow. 
    After you update and save the file eject the device and do a power cycle this should allow you to see the ip 

    [NETWORK]
    hostname = pluto
    ipaddr = 172.169.2.3
    ipaddr_host = 172.169.2.10
    netmask = 255.255.255.0

    [WLAN]
    ssid_wlan =
    pwd_wlan =
    ipaddr_wlan =

    [USB_ETHERNET]
    ipaddr_eth =
    netmask_eth = 255.255.255.0

    [SYSTEM]
    xo_correction =
    udc_handle_suspend = 0

    [ACTIONS]
    diagnostic_report = 0
    dfu = 0
    reset = 0
    calibrate = 0

  • iio_attr --uri usb:3.12.5  -C fw_version                                                                                     1 ✘ 
    fw_version: v0.39

    iio_info -u ip:192.168.2.1                                                                                                     Heavy check mark  
    Unable to create IIO context ip:192.168.2.1: Connection timed out (110)

    New config.txt as you mentioned above.

    iio_info -u ip:172.169.2.3                                                                                                     Heavy check mark  
    Unable to create IIO context ip:172.169.2.3: Connection timed out (110)
       ~                                                              

  • Can you try to change the USB Ethernet compatibility mode like explained here ?

  • With

    • blank
    • rndis
    • ncm
    • ecm

    all 

    [cs@Mini-IT13 ~]$ iio_info -u ip:172.169.2.3   
    Unable to create IIO context ip:172.169.2.3: Connection timed out (110)

Reply Children
  • after the configuration is done properly by ejecting make sure you disconnect and reconnect the usb cable for a restart 

  • I did this after every change. Nothing changed.

  • Here is my ifconfig

    [cs@Mini-IT13 ~]$ ifconfig  
    br-1ab76231e119: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet 172.19.0.1  netmask 255.255.0.0  broadcast 172.19.255.255
           inet6 fe80::e086:7dff:fee3:bbec  prefixlen 64  scopeid 0x20<link>
           ether e2:86:7d:e3:bb:ec  txqueuelen 0  (Ethernet)
           RX packets 3  bytes 84 (84.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 91  bytes 9299 (9.0 KiB)
           TX errors 0  dropped 2 overruns 0  carrier 0  collisions 0

    br-9983f0598889: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
           inet 172.22.0.1  netmask 255.255.0.0  broadcast 172.22.255.255
           ether 2a:06:43:97:68:51  txqueuelen 0  (Ethernet)
           RX packets 0  bytes 0 (0.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 0  bytes 0 (0.0 B)
           TX errors 0  dropped 42 overruns 0  carrier 0  collisions 0

    br-a1c9d36480db: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet 172.18.0.1  netmask 255.255.0.0  broadcast 172.18.255.255
           inet6 fe80::3c53:8bff:fe2c:8726  prefixlen 64  scopeid 0x20<link>
           ether 3e:53:8b:2c:87:26  txqueuelen 0  (Ethernet)
           RX packets 775  bytes 129815 (126.7 KiB)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 915  bytes 78300 (76.4 KiB)
           TX errors 0  dropped 3 overruns 0  carrier 0  collisions 0

    br-c31a3195cb1f: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet 172.20.0.1  netmask 255.255.0.0  broadcast 172.20.255.255
           inet6 fe80::7443:feff:fed1:3027  prefixlen 64  scopeid 0x20<link>
           ether 76:43:fe:d1:30:27  txqueuelen 0  (Ethernet)
           RX packets 3  bytes 84 (84.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 90  bytes 9237 (9.0 KiB)
           TX errors 0  dropped 3 overruns 0  carrier 0  collisions 0

    br-f661b67932d9: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
           inet 172.21.0.1  netmask 255.255.0.0  broadcast 172.21.255.255
           ether 3e:e1:68:73:73:6f  txqueuelen 0  (Ethernet)
           RX packets 0  bytes 0 (0.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 0  bytes 0 (0.0 B)
           TX errors 0  dropped 42 overruns 0  carrier 0  collisions 0

    docker0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
           inet 172.17.0.1  netmask 255.255.0.0  broadcast 172.17.255.255
           ether 1e:cd:00:bf:1b:04  txqueuelen 0  (Ethernet)
           RX packets 0  bytes 0 (0.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 0  bytes 0 (0.0 B)
           TX errors 0  dropped 42 overruns 0  carrier 0  collisions 0

    enp0s20f0u5u4u4: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           ether 00:e0:22:9f:1c:c5  txqueuelen 1000  (Ethernet)
           RX packets 39  bytes 5356 (5.2 KiB)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 0  bytes 0 (0.0 B)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet 192.168.178.10  netmask 255.255.255.0  broadcast 192.168.178.255
           inet6 fe80::733c:eb20:ddd6:539f  prefixlen 64  scopeid 0x20<link>
           inet6 2a02:908:1064:50c0:df5b:df6f:7b75:bbb1  prefixlen 64  scopeid 0x0<global>
           inet6 fd00::6966:8660:802e:39b  prefixlen 64  scopeid 0x0<global>
           ether 38:f7:cd:c7:4b:8c  txqueuelen 1000  (Ethernet)
           RX packets 178712  bytes 105697312 (100.8 MiB)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 94752  bytes 40735095 (38.8 MiB)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
           device memory 0x6c300000-6c3fffff   

    lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536
           inet 127.0.0.1  netmask 255.0.0.0
           inet6 ::1  prefixlen 128  scopeid 0x10<host>
           loop  txqueuelen 1000  (Local Loopback)
           RX packets 1404  bytes 1319626 (1.2 MiB)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 1404  bytes 1319626 (1.2 MiB)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    veth125d805: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet6 fe80::c420:76ff:fe7a:326a  prefixlen 64  scopeid 0x20<link>
           ether c6:20:76:7a:32:6a  txqueuelen 0  (Ethernet)
           RX packets 3  bytes 126 (126.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 148  bytes 15038 (14.6 KiB)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    veth23ca42c: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet6 fe80::582f:6eff:fed0:ddfa  prefixlen 64  scopeid 0x20<link>
           ether 5a:2f:6e:d0:dd:fa  txqueuelen 0  (Ethernet)
           RX packets 3  bytes 126 (126.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 149  bytes 15100 (14.7 KiB)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    vethe5b6f5e: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet6 fe80::f8d6:88ff:fedf:628d  prefixlen 64  scopeid 0x20<link>
           ether fa:d6:88:df:62:8d  txqueuelen 0  (Ethernet)
           RX packets 775  bytes 140665 (137.3 KiB)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 973  bytes 84101 (82.1 KiB)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    vmnet1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet 172.16.1.1  netmask 255.255.255.0  broadcast 172.16.1.255
           inet6 fe80::250:56ff:fec0:1  prefixlen 64  scopeid 0x20<link>
           ether 00:50:56:c0:00:01  txqueuelen 1000  (Ethernet)
           RX packets 0  bytes 0 (0.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 432  bytes 0 (0.0 B)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    vmnet8: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
           inet 192.168.120.1  netmask 255.255.255.0  broadcast 192.168.120.255
           inet6 fe80::250:56ff:fec0:8  prefixlen 64  scopeid 0x20<link>
           ether 00:50:56:c0:00:08  txqueuelen 1000  (Ethernet)
           RX packets 0  bytes 0 (0.0 B)
           RX errors 0  dropped 0  overruns 0  frame 0
           TX packets 105  bytes 0 (0.0 B)
           TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0