Post Go back to editing

I'm not on 192.168.2.*

Category: Software

My home network is 192.168.178.* and I can't access my Pluto via ssh with USB under 192.168.2.1. I'm running with Linux. My routers adress is  192.168.178.1. I tried different settings. My actual config.txt is:

# Analog Devices PlutoSDR Rev.C (Z7010-AD9363)
# Device Configuration File
# 1. Open with an Editor
# 2. Edit this file
# 3. Save this file on the device USB drive
# 4. Eject the device USB Drive
# Doc: wiki.analog.com/.../customizing

[NETWORK]
hostname = pluto
ipaddr = 192.168.178.190
ipaddr_host = 192.168.178.1
netmask = 255.255.255.0

[WLAN]
ssid_wlan = MyWLAN
pwd_wlan = xxxxxxxxxx
ipaddr_wlan = 192.168.178.190

[USB_ETHERNET]
ipaddr_eth = 192.168.178.190
netmask_eth = 255.255.255.0

[SYSTEM]
xo_correction =
udc_handle_suspend = 0
# USB Communication Device Class Compatibility Mode [rndis|ncm|ecm]
usb_ethernet_mode = ncm

[ACTIONS]
diagnostic_report = 0
dfu = 0
reset = 0
calibrate = 0

Thanks for your help in advance!

Edit Notes

added router adress
[edited by: gatonero at 2:32 PM (GMT -4) on 9 May 2025]
Parents
  • Hello, 

    Can you check if the drivers are installed there are detailed steps on how to do this here 

  • Everything is installed.

    iio_info -s  
    Available contexts:
           0: (mt7921_phy0,hidpp_battery_0,acpitz,hidpp_battery_1,coretemp,nvme on Default string) [local:]
           1: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=10447318ac0f0011060036002b8c172932 [usb:3.9.5]

  • Seems like it only sees the usb. 
    Considering your router ip is 192.168.178.1 can you try these settings 

    [NETWORK]
    hostname = pluto
    ipaddr = 192.168.178.2
    ipaddr_host = 192.168.178.1
    netmask = 255.255.255.0

    [WLAN]
    ssid_wlan = 
    pwd_wlan = 
    ipaddr_wlan = 

    [USB_ETHERNET]
    ipaddr_eth = 
    netmask_eth = 255.255.255.0

    [SYSTEM]
    xo_correction =
    udc_handle_suspend = 0
    # USB Communication Device Class Compatibility Mode [rndis|ncm|ecm]
    usb_ethernet_mode = ncm

    [ACTIONS]
    diagnostic_report = 0
    dfu = 0
    reset = 0
    calibrate = 0

    if this does not work can you try to connect using usb connection just to make sure you are able to access Pluto ?

Reply
  • Seems like it only sees the usb. 
    Considering your router ip is 192.168.178.1 can you try these settings 

    [NETWORK]
    hostname = pluto
    ipaddr = 192.168.178.2
    ipaddr_host = 192.168.178.1
    netmask = 255.255.255.0

    [WLAN]
    ssid_wlan = 
    pwd_wlan = 
    ipaddr_wlan = 

    [USB_ETHERNET]
    ipaddr_eth = 
    netmask_eth = 255.255.255.0

    [SYSTEM]
    xo_correction =
    udc_handle_suspend = 0
    # USB Communication Device Class Compatibility Mode [rndis|ncm|ecm]
    usb_ethernet_mode = ncm

    [ACTIONS]
    diagnostic_report = 0
    dfu = 0
    reset = 0
    calibrate = 0

    if this does not work can you try to connect using usb connection just to make sure you are able to access Pluto ?

Children
  • Seems that there is the same result:

    iio_info -s                                                                                                                    Heavy check mark  
    Available contexts:
           0: (mt7921_phy0,hidpp_battery_0,acpitz,hidpp_battery_1,coretemp,nvme on Default string) [local:]
           1: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=10447318ac0f0011060036002b8c172932 [usb:3.9.5]

    But there are three new files: 

    1. ipaddr-usb0, which is empty
    2. status, content: "here 1:"
    3. SUCCESS_ENV_UPDATE, which is empty also

    These files disapear after a reboot.

  • can you run iio_info -u ip:192.168.178.2 
    To check if we are able to see the context like this ? 

  • iio_info -u ip:192.168.178.2                                                                                                   Heavy check mark  
    Unable to create IIO context ip:192.168.178.2: Connection refused (111)

  • can you try to make a firmware update following the instructions here and then try again to configure your custom ip config ? 

  • On 192.168.178.2 there was a repeater. The repeater is now offline and I removes it's settings in my router. Now:

    iio_info -u ip:192.168.178.2                                                                                          1 ✘  3s   
    Unable to create IIO context ip:192.168.178.2: No route to host (113)

  • For now try to update the firmware.
    After the update try to run iio_info -u ip:192.168.2.1 with no other changes made. 

  • If this does not work use the config file bellow. 
    After you update and save the file eject the device and do a power cycle this should allow you to see the ip 

    [NETWORK]
    hostname = pluto
    ipaddr = 172.169.2.3
    ipaddr_host = 172.169.2.10
    netmask = 255.255.255.0

    [WLAN]
    ssid_wlan =
    pwd_wlan =
    ipaddr_wlan =

    [USB_ETHERNET]
    ipaddr_eth =
    netmask_eth = 255.255.255.0

    [SYSTEM]
    xo_correction =
    udc_handle_suspend = 0

    [ACTIONS]
    diagnostic_report = 0
    dfu = 0
    reset = 0
    calibrate = 0

  • iio_attr --uri usb:3.12.5  -C fw_version                                                                                     1 ✘ 
    fw_version: v0.39

    iio_info -u ip:192.168.2.1                                                                                                     Heavy check mark  
    Unable to create IIO context ip:192.168.2.1: Connection timed out (110)

    New config.txt as you mentioned above.

    iio_info -u ip:172.169.2.3                                                                                                     Heavy check mark  
    Unable to create IIO context ip:172.169.2.3: Connection timed out (110)
       ~                                                              

  • Can you try to change the USB Ethernet compatibility mode like explained here ?

  • With

    • blank
    • rndis
    • ncm
    • ecm

    all 

    [cs@Mini-IT13 ~]$ iio_info -u ip:172.169.2.3   
    Unable to create IIO context ip:172.169.2.3: Connection timed out (110)