Post Go back to editing

ADALM2000 DC Sweep

Thread Summary

The user is trying to perform a DC voltage sweep from -2V to 2V with a 1mV step using the ADALM2000 and Scopy software. The final answer provides a Python example for generating a DC sweep and references the libm2k bindings and examples folders for further guidance. The user also inquired about setting up libm2k and the possibility of a singular sweep rather than a continuous one.
AI Generated Content
Category: Software
Product Number: ADALM2000
Software Version: Scopy

Hi, 

I'm trying to use the ADALM2000 for a DC voltage sweep from -2V to 2V with a 1mV step. I was wondering what the best way to do that was. I'm currently trying with the Scopy software but am unsure where to start.