Post Go back to editing

Unbricking PlutoSDR in 2024

Thread Summary

The user attempted to unbrick a PlutoSDR Rev C/D using the official guide but encountered issues with serial communication and DFU mode. The solution involved running `dfu-util` as root (with `sudo`) to resolve a permissions error, which allowed the Pluto to enter DFU mode and be restored. The user also noted that the `JTAG BOOT` jumper should not be used, and the UART output should be monitored from the ADALM-UARTJTAG USB port at 115200 baud.
AI Generated Content
Category: Hardware
Product Number: ADALM-PLUTO

Hi all, I am following the official Unbricking PlutoSDR wiki guide on a bricked Pluto, however as this guide is quite outdated, here I describe my attempt at unsuccessfully unbricking a Pluto.  The hardware was handed to me after a team of satellite engineers had difficulty unbricking it, so I am not sure how a working unit should appear.  My configuration is:

Following the steps of the guide as follows:

> After the JTAG programmer is connected, provide power to PlutoSDR using either of its USB connectors. Once powered the D5 led should illuminate to signal the JTAG connection to the programmer is alive.

With the 10-way JTAG ribbon cable connected, I power the JTAG-HS3, then power the PlutoSDR (USB port "P3" plugged in to the PC, as shown in the guide figure).  The red LED labeled "VIO" lights on the UARTJTAG board.  My Pluto dimly lights the LED with designator DS2 (the one in the corner of the PCB).  The Pluto LED DS1 remains off.

> 1. Plug in JTAG as documented above into Pluto and verify you can connect with Vivado

I run:

$ source /tools/Xilinx/Vivado/2024.1/settings64.sh
$ xsct

****** Software Commandline Tool (XSCT) v2024.1.2
  **** SW Build 0 on 2024-09-05-05:57:41
    ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
    ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.


Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
         Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.


xsct% connect -host localhost -port 3121
Connection refused
xsct% 

With the command having failed, I launch the `vivado` GUI from the command line and click on the "Open Hardware Manager" task link, then Menu -> Tools -> Open new target.  Connect to local server.  The `xilinx_tcf` hardware target is auto-detected with JTAG frequency 15000000 and hardware devices `arm_dap_0` and `xc7z010_1` are auto-detected.  Hardware server settings on next page reads `localhost:3121`.  Closing the dialog, the hardware list shows the status of `arm_dap_0` as "N/A", and the status of `xc7x010_1` as "Not programmed".

Now trying again with the command line, I get

$ xsct

****** Software Commandline Tool (XSCT) v2024.1.2
  **** SW Build 0 on 2024-09-05-05:57:41
    ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
    ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.


Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
         Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.


xsct% connect -host localhost -port 3121
tcfchan#0
xsct% targets
  1  APU
     2  ARM Cortex-A9 MPCore #0 (Running)
     3  ARM Cortex-A9 MPCore #1 (Running)
  4  xc7z010
xsct% 

There must be a command that is missing from the command line instructions, but now the command appears to work after the GUI procedure I described.

> 2. Download the JTAG bootstrap zip from the firmware release page (plutosdr-jtag-bootstrap-<Firmware Version>.zip)

> 3. Unzip the zip then source the run.tcl inside with xmd from the Xilinx tools (xmd -tcl run.tcl). We are done with JTAG now

The command `xmd` no longer exists, however the zip file contains a clue in the form of a file called `run-xsdb.tcl` with contents that look similar to the `run.tcl` in the instructions.  The command to run is found in the file comment.  Presumably, `xsdb` is a replacement for `xmd`.

~/Downloads/plutosdr-jtag-bootstrap-v0.39$ xsdb run-xsdb.tcl
attempting to launch hw_server

****** Xilinx hw_server v2024.1.2
  **** Build date : Aug 28 2024 at 13:40:10
    ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
    ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.

INFO: hw_server application started
INFO: Use Ctrl-C to exit hw_server application

INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121

$

The command prompt returns without any explicit success message but no error neither.  LEDs are same as before.  The instruction reads "We are done with JTAG now", but not sure what that means, whether we should leave it plugged in or unplug it.  (spoiler: it made no difference in my case).  For what it's worth, I left it plugged in and considered it "done".

> 4. Next plugin a USB cable to the UART port of the ADALM-UARTJTAG connector and open a serial session (Putty or screen or …)

A green LED (labeled "VUSB") lights up on the ADALM-UARTJTAG when plugged in as described.  The guide doesn't give any details about what baud, stop bits, parity etc are needed, however despite trying virtually all possible common serial baud rate speeds and parameters, I was unable to get any sign of life from the serial port, and no u-boot menu was seen as indicated on the next step of the procedure.

Notably, after running the `xsdb` tcl script causes subsequent connection attempts with `xsct` to fail.  Heading back to the GUI and reconnecting to the JTAG-HS3, the Xilinx still shows as "Not programmed".

After turning it off and on again, I reconnect with the GUI as before, except this time I click "Program device" with the bitstream file `system_top.bit`.  There appears to be no "Debug probes file", however this does not seem to prevent the programming from going ahead.  It appears to succeed, listing `arm_dap_0` as "N/A" (as before) but now `xc7x010_1` shows as "Programmed" and now the DS1 LED lights up much brighter than the constantly lit dim DS2 led.  Despite this promising sign of life, u-boot remains unseen on any serial port with any baud rate and parameters I have tried, repeatedly typing, sending CTRL+C, and hitting ENTER with no result (to both Pluto and JTAG serial ports).  There appears to be a `u-boot.elf` file in the zip archive, but I haven't yet found a way to get this onto the board by the command line or the GUI.  Typing the tcl script lines one by one appears to

Can anyone spot where it's going wrong, or if it may even be a sign of dead Pluto?

It would really benefit the community to at least update that official unbricking guide, even if only to instill us with some confidence that the guide isn't broken and that we're not doing anything wrong.  It would help with:

  • specifying the serial parameters (baud rate, stop bits, parity etc) needed to open the serial session (and whether it's to the Pluto's serial or the JTAG's serial)
  • whether the JTAG should be unplugged
  • a working command line procedure to connect to the debugger first time with `xsct` that doesn't rely on the GUI
  • update the `xmd` command to `xsdb` (or whatever the correct command is)
  • some links to the zip file in the guide would be helpful

I am still hoping to get myself back into HDL/FPGA/SDR development after this thing is unbricked.

Parents
  • Hi  ,
    Indeed the command xmd no longer exists, the valid one is "xsct run.tcl"

    In regards to the UART parameters: https://wiki.analog.com/resources/fpga/uart_setup
    However, when going trough the steps this has been observed:
    - after programming the bootloader with "xsct run.tcl" there is output on the UART (uboot boot log)
    - pluto then boots dirrectly into DFU mode, step 5 "run dfu_sf" is not needed

    I've observed the same behaviour, the UART is not responding after flashing with run.tcl as Pluto is already in DFU mode.
    I guess that your pluto is recoverable and in DFU.

    Also, when I tried this, disconnecting and reconnecting power to the pluto after "xsct run.tcl" did not seem to make it boot back to DFU, so it's possible that you will need to run "xsct run.tcl" again.

  • Hi Dumitru, thanks for the suggestions, however running `xsct run.tcl` also failed for me:

    ~$ source /tools/Xilinx/Vivado/2024.1/settings64.sh
    ~$ cd Downloads/plutosdr-jtag-bootstrap-v0.39/
    ~/Downloads/plutosdr-jtag-bootstrap-v0.39$ ls
    ps7_init.tcl  run.tcl  run-xsdb.tcl  system_top.bit  u-boot.elf
    ~/Downloads/plutosdr-jtag-bootstrap-v0.39$ xsct run.tcl
    unexpected arguments: arm hw
        while executing
    "error "unexpected arguments: $arglist""
        (procedure "::xsdb::get_options" line 69)
        invoked from within
    "::xsdb::get_options args $options"
        (procedure "connect" line 17)
        invoked from within
    "connect arm hw"
        (file "run.tcl" line 7)
    

    I also tried going through the standard DFU procedure both with and without flashing `system_top.bit` from the GUI however:

    • all of their `iio_attr`, `dfu-util` and `lsusb` commands I have installed but all of them failed to identify the Pluto
    • a mass storage device did not appear on my computer
    • there was no additional network device hardware detected
    • and `dmesg` didn't report any changes

    As before, I tried `xsct` and each step of the DFU procedure both with and without flashing the bitstream file from the GUI (as described in the opening post) and from each of the USB ports, while monitoring any serial port with the correct serial parameters but still nothing so far.

  • Thanks Dumitru, I checked the following things (and some steps from the DFU guide) but still can't seem to get it in the right mode it needs to be in:

    • an `lsusb` was performed after each step before and after `xsct`.  The only times a new USB device was detected was when the JTAG-HS3 and (optionally) the UARTJTAG was plugged in.  The name "Analog Devices" was not found, nor was the VID 0456.
    • `iio_attr -a -C fw_version` printed `No IIO context found.`
    • `sudo dfu-util --list` shows nothing listed (tried a few times)
    • Tried with and without unplugging the 10-pin JTAG cable from the Pluto after the `xsct` process
    • Tried with and without opening the UARTJTAG serial port (not the Pluto on-board FTDI on the right USB socket)
    • Tried pressing the device button with a toothpick after
    • Tried the Pluto USB port that I normally try on the left ("P2"), as well as the port on the right ("P3")
    • No new mass storage devices appeared at any time
    • The LEDs showed the same each time.  The left LED ("DS2") lights dimly, while the right LED ("DS1") remains off.

    Paul

  • Did you test this with 'JTAG BOOT' jumper on the UARTJTAG plugged in?

    You should see some output on the UART from the ADALM-UARTJTAG usb port when power-cycling the Pluto if the device boots into DFU. 

    U-Boot PlutoSDR v0.20-PlutoSDR-00066-g90401ce9ce (Nov 17 2023 - 10:28:18 +0100)
    
    I2C:   ready
    DRAM:  ECC disabled 512 MiB
    SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB
    In:    serial@e0001000
    Out:   serial@e0001000
    Err:   serial@e0001000
    Model: Zynq Pluto SDR Board
    Hit any key to stop autoboot:  0 
    Booting silently
    BOOT failed entering DFU mode ...
    SF: Locked
    gpio: pin 15 (gpio 15) value is 1
    Entering DFU SF mode ...

  • The last steps were done without the 'JTAG BOOT' jumper, but I tried it again with the jumper and still nothing seen on the UARTJTAG's USB UART at 115200 baud.

    I also tried power-cycling the Pluto after flashing while keeping the 10-pin ribbon and UARTJTAG connected (and both with and without JTAG-HS3 connected) but again, nothing seen on the UARTJTAG USB UART still unfortunately.

  • Note also, probing the RX test point near the JTAG header on the Pluto with an oscilloscope shows characters being sent in from the computer to the Pluto when typed in the serial terminal at 115200, but probing TX during and after flashing (and also power cycling) shows no characters being sent from the Pluto to the computer (should be U-boot messages).

  • Hi,

    Some ideas.

    The JTAG BOOT jumper should not connected.

    1. Use a second USB cable to power the Pluto on the power input micro USB. In case your main USB or power source is not reliable/sufficient.

    2. You can use the system_top.xsa to create a "Hello World" app. That will let you know if the is any problem with the UART/FPGA.
    maybe add some other code and some break points. To see if the zynq behaves as expected, if not, than that SoC can RIP.

    Andrei

  • Hi Anrdei,

    I tried a second USB cable to a USB plug-in charger in addition to the main port to the computer, but still nothing on the UARTJTAG USB serial (without JTAG BOOT jumper).

    Searching for `system_top.xsa`, I came across building boot images - so is `system_top.xsa` an image that I generate from Vivado/Vitis/HDL code?  Maybe it results in a `system_top.bit` file?  Unfortunately, I haven't used a working Pluto or Xilinx tools beyond these unbricking attempts.

    I can program the `system_top.bit` that came with the bootstrap zip separately from the GUI which causes the DS1 LED to light bright.  Separately, I can program `u-boot.bin` from `xsct`.  It all seems so close yet no serial output in either case.

    I'll try to create a hello world project some time and will update whether it worked, but for now my Pluto is looking quite dead.

  • Hi,

    From where you got the bootstrap files you can get an archive with all the files used for the firmware.
    https://github.com/analogdevicesinc/plutosdr-fw/releases/tag/v0.39

    plutosdr-fw-v0.39.zip

    There you can find the system_top.xsa file which you can use to create your hardware platform in Vitis.
    The xsa is the result of the hdl build. It is an archive containing the bitstream and other info related to the zynq and the rest of the bits and stuff.

    You can find a lot of examples on you to create a hello world design for a custom design(xsa file).

    Andrei

  • Thanks Andrei, I'll look into it and give this a try when I return next week... I'll update you.  Paul

  • Hi m0set,

    I've encountered similar problems. Do you have luck now?

    MUN

  • I'm having the same symptoms and have done most of the same experiments trying to unbrick a Pluto. Any news? Did you find a way?

Reply Children
  • If you described what have you tried and with what, some results/errors, we can try to help you solve it.

    Andrei

  • I won't attempt to repeat the amazingly thorough recitation of results that m0set provided in the thread above. I had what seemed like indistinguishable results.

    However, I was able to get back control of my Pluto. In my case, the problem was that I did not realize that dfu-util needs to be run as root (with sudo) on the host machine. I found this surprising, because the operation is one that seems privileged only on the target device, and not on the host device. In the tutorials and documentation I read, there was no strong emphasis given to this requirement. Worse, the dfu-util program never gave any diagnostic message about permissions or any hint that it was restricted from operating on the target device. It just gave wrong results like this:

    dfu-util: Device has DFU interface, but has no DFU functional descriptor
    
    Deducing device DFU version from functional descriptor length
    
    dfu-util: Cannot open DFU device 0456:b674 found on devnum 44 (LIBUSB_ERROR_ACCESS)

    In retrospect I see now that "LIBUSB_ERROR_ACCESS" was trying to tell me about the permissions problem, but on first reading it seemed that the host was successfully talking to the DFU target, but that it was getting back results pointing to a problem with the DFU support in the target.

    Once I noticed that dfu-util needed privileges to work correctly, I found that entering DFU mode using the button on the Pluto was working after all, and I was able to follow the rest of the instructions in the wiki article wiki.analog.com/university/tools/pluto/users/firmware under "Debugging DFU" to restore my Pluto.

    As a side note, the privileges dfu-util needs are probably better granted with a udev rule than with sudo, but I couldn't find any documentation suggesting that. Possibly this is on purpose, since a suggested udev rule would be even easier to overlook than the use of sudo to run dfu-util commands.

    My problem is solved. I hope this message helps others to solve theirs.

      -Paul