Post Go back to editing

Unbricking PlutoSDR in 2024

Thread Summary

The user attempted to unbrick a PlutoSDR Rev C/D using the official guide but encountered issues with serial communication and DFU mode. The solution involved running `dfu-util` as root (with `sudo`) to resolve a permissions error, which allowed the Pluto to enter DFU mode and be restored. The user also noted that the `JTAG BOOT` jumper should not be used, and the UART output should be monitored from the ADALM-UARTJTAG USB port at 115200 baud.
AI Generated Content
Category: Hardware
Product Number: ADALM-PLUTO

Hi all, I am following the official Unbricking PlutoSDR wiki guide on a bricked Pluto, however as this guide is quite outdated, here I describe my attempt at unsuccessfully unbricking a Pluto.  The hardware was handed to me after a team of satellite engineers had difficulty unbricking it, so I am not sure how a working unit should appear.  My configuration is:

Following the steps of the guide as follows:

> After the JTAG programmer is connected, provide power to PlutoSDR using either of its USB connectors. Once powered the D5 led should illuminate to signal the JTAG connection to the programmer is alive.

With the 10-way JTAG ribbon cable connected, I power the JTAG-HS3, then power the PlutoSDR (USB port "P3" plugged in to the PC, as shown in the guide figure).  The red LED labeled "VIO" lights on the UARTJTAG board.  My Pluto dimly lights the LED with designator DS2 (the one in the corner of the PCB).  The Pluto LED DS1 remains off.

> 1. Plug in JTAG as documented above into Pluto and verify you can connect with Vivado

I run:

$ source /tools/Xilinx/Vivado/2024.1/settings64.sh
$ xsct

****** Software Commandline Tool (XSCT) v2024.1.2
  **** SW Build 0 on 2024-09-05-05:57:41
    ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
    ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.


Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
         Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.


xsct% connect -host localhost -port 3121
Connection refused
xsct% 

With the command having failed, I launch the `vivado` GUI from the command line and click on the "Open Hardware Manager" task link, then Menu -> Tools -> Open new target.  Connect to local server.  The `xilinx_tcf` hardware target is auto-detected with JTAG frequency 15000000 and hardware devices `arm_dap_0` and `xc7z010_1` are auto-detected.  Hardware server settings on next page reads `localhost:3121`.  Closing the dialog, the hardware list shows the status of `arm_dap_0` as "N/A", and the status of `xc7x010_1` as "Not programmed".

Now trying again with the command line, I get

$ xsct

****** Software Commandline Tool (XSCT) v2024.1.2
  **** SW Build 0 on 2024-09-05-05:57:41
    ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
    ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.


Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
         Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.


xsct% connect -host localhost -port 3121
tcfchan#0
xsct% targets
  1  APU
     2  ARM Cortex-A9 MPCore #0 (Running)
     3  ARM Cortex-A9 MPCore #1 (Running)
  4  xc7z010
xsct% 

There must be a command that is missing from the command line instructions, but now the command appears to work after the GUI procedure I described.

> 2. Download the JTAG bootstrap zip from the firmware release page (plutosdr-jtag-bootstrap-<Firmware Version>.zip)

> 3. Unzip the zip then source the run.tcl inside with xmd from the Xilinx tools (xmd -tcl run.tcl). We are done with JTAG now

The command `xmd` no longer exists, however the zip file contains a clue in the form of a file called `run-xsdb.tcl` with contents that look similar to the `run.tcl` in the instructions.  The command to run is found in the file comment.  Presumably, `xsdb` is a replacement for `xmd`.

~/Downloads/plutosdr-jtag-bootstrap-v0.39$ xsdb run-xsdb.tcl
attempting to launch hw_server

****** Xilinx hw_server v2024.1.2
  **** Build date : Aug 28 2024 at 13:40:10
    ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
    ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.

INFO: hw_server application started
INFO: Use Ctrl-C to exit hw_server application

INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121

$

The command prompt returns without any explicit success message but no error neither.  LEDs are same as before.  The instruction reads "We are done with JTAG now", but not sure what that means, whether we should leave it plugged in or unplug it.  (spoiler: it made no difference in my case).  For what it's worth, I left it plugged in and considered it "done".

> 4. Next plugin a USB cable to the UART port of the ADALM-UARTJTAG connector and open a serial session (Putty or screen or …)

A green LED (labeled "VUSB") lights up on the ADALM-UARTJTAG when plugged in as described.  The guide doesn't give any details about what baud, stop bits, parity etc are needed, however despite trying virtually all possible common serial baud rate speeds and parameters, I was unable to get any sign of life from the serial port, and no u-boot menu was seen as indicated on the next step of the procedure.

Notably, after running the `xsdb` tcl script causes subsequent connection attempts with `xsct` to fail.  Heading back to the GUI and reconnecting to the JTAG-HS3, the Xilinx still shows as "Not programmed".

After turning it off and on again, I reconnect with the GUI as before, except this time I click "Program device" with the bitstream file `system_top.bit`.  There appears to be no "Debug probes file", however this does not seem to prevent the programming from going ahead.  It appears to succeed, listing `arm_dap_0` as "N/A" (as before) but now `xc7x010_1` shows as "Programmed" and now the DS1 LED lights up much brighter than the constantly lit dim DS2 led.  Despite this promising sign of life, u-boot remains unseen on any serial port with any baud rate and parameters I have tried, repeatedly typing, sending CTRL+C, and hitting ENTER with no result (to both Pluto and JTAG serial ports).  There appears to be a `u-boot.elf` file in the zip archive, but I haven't yet found a way to get this onto the board by the command line or the GUI.  Typing the tcl script lines one by one appears to

Can anyone spot where it's going wrong, or if it may even be a sign of dead Pluto?

It would really benefit the community to at least update that official unbricking guide, even if only to instill us with some confidence that the guide isn't broken and that we're not doing anything wrong.  It would help with:

  • specifying the serial parameters (baud rate, stop bits, parity etc) needed to open the serial session (and whether it's to the Pluto's serial or the JTAG's serial)
  • whether the JTAG should be unplugged
  • a working command line procedure to connect to the debugger first time with `xsct` that doesn't rely on the GUI
  • update the `xmd` command to `xsdb` (or whatever the correct command is)
  • some links to the zip file in the guide would be helpful

I am still hoping to get myself back into HDL/FPGA/SDR development after this thing is unbricked.

Parents
  • Hi  ,
    Indeed the command xmd no longer exists, the valid one is "xsct run.tcl"

    In regards to the UART parameters: https://wiki.analog.com/resources/fpga/uart_setup
    However, when going trough the steps this has been observed:
    - after programming the bootloader with "xsct run.tcl" there is output on the UART (uboot boot log)
    - pluto then boots dirrectly into DFU mode, step 5 "run dfu_sf" is not needed

    I've observed the same behaviour, the UART is not responding after flashing with run.tcl as Pluto is already in DFU mode.
    I guess that your pluto is recoverable and in DFU.

    Also, when I tried this, disconnecting and reconnecting power to the pluto after "xsct run.tcl" did not seem to make it boot back to DFU, so it's possible that you will need to run "xsct run.tcl" again.

Reply
  • Hi  ,
    Indeed the command xmd no longer exists, the valid one is "xsct run.tcl"

    In regards to the UART parameters: https://wiki.analog.com/resources/fpga/uart_setup
    However, when going trough the steps this has been observed:
    - after programming the bootloader with "xsct run.tcl" there is output on the UART (uboot boot log)
    - pluto then boots dirrectly into DFU mode, step 5 "run dfu_sf" is not needed

    I've observed the same behaviour, the UART is not responding after flashing with run.tcl as Pluto is already in DFU mode.
    I guess that your pluto is recoverable and in DFU.

    Also, when I tried this, disconnecting and reconnecting power to the pluto after "xsct run.tcl" did not seem to make it boot back to DFU, so it's possible that you will need to run "xsct run.tcl" again.

Children
  • Hi Dumitru, thanks for the suggestions, however running `xsct run.tcl` also failed for me:

    ~$ source /tools/Xilinx/Vivado/2024.1/settings64.sh
    ~$ cd Downloads/plutosdr-jtag-bootstrap-v0.39/
    ~/Downloads/plutosdr-jtag-bootstrap-v0.39$ ls
    ps7_init.tcl  run.tcl  run-xsdb.tcl  system_top.bit  u-boot.elf
    ~/Downloads/plutosdr-jtag-bootstrap-v0.39$ xsct run.tcl
    unexpected arguments: arm hw
        while executing
    "error "unexpected arguments: $arglist""
        (procedure "::xsdb::get_options" line 69)
        invoked from within
    "::xsdb::get_options args $options"
        (procedure "connect" line 17)
        invoked from within
    "connect arm hw"
        (file "run.tcl" line 7)
    

    I also tried going through the standard DFU procedure both with and without flashing `system_top.bit` from the GUI however:

    • all of their `iio_attr`, `dfu-util` and `lsusb` commands I have installed but all of them failed to identify the Pluto
    • a mass storage device did not appear on my computer
    • there was no additional network device hardware detected
    • and `dmesg` didn't report any changes

    As before, I tried `xsct` and each step of the DFU procedure both with and without flashing the bitstream file from the GUI (as described in the opening post) and from each of the USB ports, while monitoring any serial port with the correct serial parameters but still nothing so far.

  • Hi  ,
    Sorry for the confusion, I meant to say "xsct run-xsdb.tcl". After running this command Pluto should boot into DFU mode.

    When Pluto is connected with usb to your PC, does the "Analog Devices, Inc. USB download gadget" device appear when running lsusb?

    Also, when booting into DFU mode, Pluto outputs a boot log to the UART port of ADALM-UARTJTAG. Test this by unplugging-plugging the USB connector that powers the Pluto.

  • Hi  ,

    I gave it another try with `xsct run-xsdb.tcl`.  The program appears to complete without any obvious error message shown however it seems (at least from the command output and its effects on the hardware) to be identical to running `xsdb run-xsdb.tcl`:

    ~$ source /tools/Xilinx/Vivado/2024.1/settings64.sh
    ~$ cd Downloads/plutosdr-jtag-bootstrap-v0.39/
    ~/Downloads/plutosdr-jtag-bootstrap-v0.39$ xsct run-xsdb.tcl 
    attempting to launch hw_server
    
    ****** Xilinx hw_server v2024.1.2
      **** Build date : Aug 28 2024 at 13:40:10
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    INFO: hw_server application started
    INFO: Use Ctrl-C to exit hw_server application
    
    INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121
    

    Tried all the ports and all the combinations as before but the result seems the same i.e., no output on serial, no mass storage, the LED DS2 remains dim and DS1 remains off etc (unlike the GUI method I described above, which gives just an inkling to suggest there is still life in the unit but has its own dead end i.e. no obvious way to run `u-boot.elf` and to see it on the serial port).

    Does your `xsct run-xsdb.tcl` output look the same as mine?

  • Hi ,

    From above it looks like the tools could not connect to the hw_server.

    Please do the following experiment.

    In a terminal on which you have the paths to AMD/Xilinx tools, enter:

    xsct
    
    connect
    
    target
    
    exit


    Andrei

  • Hi  ,

    You could also try to do the commands from 'run-xsdb.tcl' by hand and see the output from each one:
    Enter the xsct cli, then follow the commands from 'run-xsdb.tcl' but with one additional reset to the APU (target 1):

    # xsct
                                                                                                                                                                                       
    ****** Software Commandline Tool (XSCT) v2023.1.0
      **** SW Build 0 on 2023-05-03-16:48:11
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2023 Advanced Micro Devices, Inc. All Rights Reserved.
    
    
    xsct% connect                                                                                                                                                                      
    attempting to launch hw_server
                                                                                                                                                                                       
    ****** Xilinx hw_server v2023.1
      **** Build date : May  3 2023 at 14:03:27
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2023 Advanced Micro Devices, Inc. All Rights Reserved.
    
    INFO: hw_server application started
    INFO: Use Ctrl-C to exit hw_server application
    
    INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121
    
    tcfchan#0
    xsct% target                                                                                                                                                                       
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsct% target 1                                                                                                                                                                     
    xsct% rst                                                                                                                                                                          
    xsct% target 2                                                                                                                                                                     
    xsct% rst                                                                                                                                                                          
    xsct% source ps7_init.tcl
    xsct% ps7_init                                                                                                                                                                     
    xsct% ps7_post_config                                                                                                                                                              
    xsct% dow u-boot.elf                                                                                                                                                               
    Downloading Program -- /home/analog/Downloads/u-boot.elf
    	section, .text: 0x04000000 - 0x0403f613
    	section, efi_runtime_text: 0x0403f614 - 0x0403f62b
    	section, .rodata: 0x0403f630 - 0x0404f873
    	section, .hash: 0x0404f874 - 0x0404f88b
    	section, .dtb.init.rodata: 0x0404f890 - 0x04051c4f
    	section, .data: 0x04051c50 - 0x04053e77
    	section, .got.plt: 0x04053e78 - 0x04053e83
    	section, efi_runtime_data: 0x04053e88 - 0x04053f4f
    	section, .u_boot_list: 0x04053f50 - 0x04054d53
    	section, .rel.dyn: 0x04054d54 - 0x0405d7b3
    	section, .bss_start: 0x04054d54 - 0x04054d53
    	section, .bss: 0x04054d54 - 0x040a5793
    	section, .bss_end: 0x040a5794 - 0x040a5793
    100%    0MB   0.5MB/s  00:00                                                                                                                                                       
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /home/analog/Downloads/u-boot.elf
    xsct% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)


    If you get the error:
    Memory write error at 0xF8000778. Cannot flush JTAG server queue. ftdi_read_data failed: usb bulk read failed  

    Try to reset targets 1 and 2 again then continue with the following instructions.
    After running the commands, Pluto should be in DFU mode.

    Dumitru

  • Thanks , it seems my hardware is indeed recognized with `xsct`:

    ~$ source /tools/Xilinx/Vivado/2024.1/settings64.sh
    ~$ xsct
    rlwrap: warning: your $TERM is 'xterm-256color' but rlwrap couldn't find it in the terminfo database. Expect some problems.
                                                                                                                                                                  
    ****** Software Commandline Tool (XSCT) v2024.1.2
      **** SW Build 0 on 2024-09-05-05:57:41
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    
    Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
             Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.
    
    
    xsct% connect                                                                                                                                                 
    attempting to launch hw_server                                                                                                                                
                                                                                                                                                                  
    ****** Xilinx hw_server v2024.1.2
      **** Build date : Aug 28 2024 at 13:40:10
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    INFO: hw_server application started
    INFO: Use Ctrl-C to exit hw_server application
    
    INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121
    
    tcfchan#0
    xsct% target                                                                                                                                                  
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsct% exit                                                                                                                                                    
    exit
    

  • Hi  

    I did manage to type in the commands but still nothing on the serial output.  Here's my method:

    • Have the JTAG-HS3 connected to ADALM-UARTJTAG and in turn connected to Pluto with 10-pin JTAG
    • Plug in JS3-HTAG USB to computer
    • Plug in the left (P2) USB port on the Pluto to computer
    • Run up to `connect` with `xsct`
    • Plug in the USB side of the ADALM-UARTJTAG and open at 115200 baud
    • Run the rest of the `xsct` commands as indicated

    Sometimes I reverse the last two steps but the same result.  Here's my output the first time:

    ~$ xsct
    rlwrap: warning: your $TERM is 'xterm-256color' but rlwrap couldn't find it in the terminfo database. Expect some problems.
                                                                                                                                                                  
    ****** Software Commandline Tool (XSCT) v2024.1.2
      **** SW Build 0 on 2024-09-05-05:57:41
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    
    Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
             Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.
    
    
    xsct% connect                                                                                                                                                 
    attempting to launch hw_server                                                                                                                                
                                                                                                                                                                  
    ****** Xilinx hw_server v2024.1.2
      **** Build date : Aug 28 2024 at 13:40:10
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    INFO: hw_server application started
    INFO: Use Ctrl-C to exit hw_server application
    
    INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121
    
    tcfchan#0
    xsct% target                                                                                                                                                  
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsct% target 1                                                                                                                                                
    xsct% rst                                                                                                                                                     
    xsct% target 2                                                                                                                                                
    xsct% rst                                                                                                                                                     
    xsct% source ps7_init.tcl                                                                                                                                     
    xsct% ps7_init                                                                                                                                                
    xsct% ps7_post_config                                                                                                                                         
    xsct% dow u-boot.elf                                                                                                                                          
    Downloading Program -- /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf                                                                         
    	section, .text: 0x04000000 - 0x0403f613
    	section, efi_runtime_text: 0x0403f614 - 0x0403f62b
    	section, .rodata: 0x0403f630 - 0x0404f873
    	section, .hash: 0x0404f874 - 0x0404f88b
    	section, .dtb.init.rodata: 0x0404f890 - 0x04051c4f
    	section, .data: 0x04051c50 - 0x04053e77
    	section, .got.plt: 0x04053e78 - 0x04053e83
    	section, efi_runtime_data: 0x04053e88 - 0x04053f4f
    	section, .u_boot_list: 0x04053f50 - 0x04054d53
    	section, .rel.dyn: 0x04054d54 - 0x0405d7b3
    	section, .bss_start: 0x04054d54 - 0x04054d53
    	section, .bss: 0x04054d54 - 0x040a5793
    	section, .bss_end: 0x040a5794 - 0x040a5793
    100%    0MB   0.2MB/s  00:01                                                                                                                                  
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf
    xsct% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0x59c (Suspended)
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running (APB AP transaction error, DAP status 0xF0000021)
    xsct% con
    Already running
    xsct% state
    APB AP transaction error, DAP status 0xF0000021
    xsct%

    Note that I'm not using the `JTAG BOOT` jumper on the UARTJTAG (it reportedly halts the Zynq and prevents U-boot finding the SPI flash as indicated in the ADALM-UARTJTAG page) but I put the jumper on anyway this time:

    ~$ xsct
    rlwrap: warning: your $TERM is 'xterm-256color' but rlwrap couldn't find it in the terminfo database. Expect some problems.
                                                                                                                                                                  
    ****** Software Commandline Tool (XSCT) v2024.1.2
      **** SW Build 0 on 2024-09-05-05:57:41
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    
    Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
             Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.
    
    
    xsct% connect                                                                                                                                                 
    attempting to launch hw_server                                                                                                                                
                                                                                                                                                                  
    ****** Xilinx hw_server v2024.1.2
      **** Build date : Aug 28 2024 at 13:40:10
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    INFO: hw_server application started
    INFO: Use Ctrl-C to exit hw_server application
    
    INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121
    
    tcfchan#0
    xsct% target                                                                                                                                                  
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsct% target 1
    xsct% rst
    xsct% target 2
    xsct% rst
    xsct% source ps7_init.tcl
    xsct% ps7_init
    xsct% ps7_post_config
    xsct% dow u-boot.elf
    Downloading Program -- /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf                                                                         
    	section, .text: 0x04000000 - 0x0403f613
    	section, efi_runtime_text: 0x0403f614 - 0x0403f62b
    	section, .rodata: 0x0403f630 - 0x0404f873
    	section, .hash: 0x0404f874 - 0x0404f88b
    	section, .dtb.init.rodata: 0x0404f890 - 0x04051c4f
    	section, .data: 0x04051c50 - 0x04053e77
    	section, .got.plt: 0x04053e78 - 0x04053e83
    	section, efi_runtime_data: 0x04053e88 - 0x04053f4f
    	section, .u_boot_list: 0x04053f50 - 0x04054d53
    	section, .rel.dyn: 0x04054d54 - 0x0405d7b3
    	section, .bss_start: 0x04054d54 - 0x04054d53
    	section, .bss: 0x04054d54 - 0x040a5793
    	section, .bss_end: 0x040a5794 - 0x040a5793
    100%    0MB   0.2MB/s  00:01                                                                                                                                  
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf
    xsct% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)                                                                              
    xsct% con                                                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running                                                                                                              
    xsct% state                                                                                                                                                   
    Running
    xsct% 

    Definitely looks like one less error but still nothing on the serial.  Trying another time with the jumper removed:

    ~$ xsct
    rlwrap: warning: your $TERM is 'xterm-256color' but rlwrap couldn't find it in the terminfo database. Expect some problems.
                                                                                                                                                                  
    ****** Software Commandline Tool (XSCT) v2024.1.2
      **** SW Build 0 on 2024-09-05-05:57:41
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    
    Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
             Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.
    
    
    xsct% connect                                                                                                                                                 
    attempting to launch hw_server                                                                                                                                
                                                                                                                                                                  
    ****** Xilinx hw_server v2024.1.2
      **** Build date : Aug 28 2024 at 13:40:10
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    INFO: hw_server application started
    INFO: Use Ctrl-C to exit hw_server application
    
    INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121
    
    tcfchan#0
    xsct% target                                                                                                                                                  
      1  APU                                                                                                                                                      
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsct% target 1                                                                                                                                                
    xsct% rst                                                                                                                                                     
    xsct% target 2                                                                                                                                                
    xsct% rst                                                                                                                                                     
    xsct% source ps7_init.tcl                                                                                                                                     
    xsct% ps7_init                                                                                                                                                
    xsct% ps7_post_config                                                                                                                                         
    xsct% dow u-boot.elf                                                                                                                                          
    Downloading Program -- /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf                                                                         
    	section, .text: 0x04000000 - 0x0403f613
    	section, efi_runtime_text: 0x0403f614 - 0x0403f62b
    	section, .rodata: 0x0403f630 - 0x0404f873
    	section, .hash: 0x0404f874 - 0x0404f88b
    	section, .dtb.init.rodata: 0x0404f890 - 0x04051c4f
    	section, .data: 0x04051c50 - 0x04053e77
    	section, .got.plt: 0x04053e78 - 0x04053e83
    	section, efi_runtime_data: 0x04053e88 - 0x04053f4f
    	section, .u_boot_list: 0x04053f50 - 0x04054d53
    	section, .rel.dyn: 0x04054d54 - 0x0405d7b3
    	section, .bss_start: 0x04054d54 - 0x04054d53
    	section, .bss: 0x04054d54 - 0x040a5793
    	section, .bss_end: 0x040a5794 - 0x040a5793
    100%    0MB   0.2MB/s  00:01                                                                                                                                  
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf
    xsct% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0x59c (Suspended)                                                                                   
    xsct% state                                                                                                                                                   
    Stopped: (Suspended)
    xsct% con                                                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running                                                                                                              
    xsct% state                                                                                                                                                   
    Running
    xsct% 

    It's "Running" according to the status but still nothing on the serial output.  Note the hex addresses are different each time so not sure what's going on there.

    I sometimes tried the `xsct` commands after flashing the `system_top.bit` from the GUI (just because it feels good when DS1 lights up bright like it's coming to life...) but the `rst` command caused the LED to turn back off.  I run it without `rst` as follows:

    ~$ xsct
    rlwrap: warning: your $TERM is 'xterm-256color' but rlwrap couldn't find it in the terminfo database. Expect some problems.
                                                                                                                                                                  
    ****** Software Commandline Tool (XSCT) v2024.1.2
      **** SW Build 0 on 2024-09-05-05:57:41
        ** Copyright 1986-2022 Xilinx, Inc. All Rights Reserved.
        ** Copyright 2022-2024 Advanced Micro Devices, Inc. All Rights Reserved.
    
    
    Warning: XSCT has been deprecated. It will still be available for several releases.It's recommended to start new projects with new python command line tool.
             Use "vitis -s <script>" (script mode) and "vitis -i" (interactive mode) to load new Python CLI for Vitis.
    
    
    xsct% target                                                                                                                                                  
    Invalid target. Use "connect" command to connect to hw_server/TCF agent                                                                                       
    xsct% connect                                                                                                                                                 
    tcfchan#0
    xsct% target                                                                                                                                                  
      1  APU                                                                                                                                                      
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsct% target 2                                                                                                                                                
    xsct% source ps7_init.tcl                                                                                                                                     
    xsct% ps7_init                                                                                                                                                
    xsct% ps7_post_config                                                                                                                                         
    xsct% dow u-boot.elf                                                                                                                                          
    Downloading Program -- /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf                                                                         
    	section, .text: 0x04000000 - 0x0403f613
    	section, efi_runtime_text: 0x0403f614 - 0x0403f62b
    	section, .rodata: 0x0403f630 - 0x0404f873
    	section, .hash: 0x0404f874 - 0x0404f88b
    	section, .dtb.init.rodata: 0x0404f890 - 0x04051c4f
    	section, .data: 0x04051c50 - 0x04053e77
    	section, .got.plt: 0x04053e78 - 0x04053e83
    	section, efi_runtime_data: 0x04053e88 - 0x04053f4f
    	section, .u_boot_list: 0x04053f50 - 0x04054d53
    	section, .rel.dyn: 0x04054d54 - 0x0405d7b3
    	section, .bss_start: 0x04054d54 - 0x04054d53
    	section, .bss: 0x04054d54 - 0x040a5793
    	section, .bss_end: 0x040a5794 - 0x040a5793
    100%    0MB   0.2MB/s  00:01                                                                                                                                  
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /home/pasha/Downloads/plutosdr-jtag-bootstrap-v0.39/u-boot.elf
    xsct% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0x59c (Suspended)                                                                                   
    xsct% state                                                                                                                                                   
    Stopped: (Suspended)
    xsct% con                                                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running                                                                                                              
    xsct% state                                                                                                                                                   
    Running
    xsct% 

    but still no serial output.  Still not giving up.  I will keep reading and trying to work it...

  • After running 'dow u-boot.elf' pluto should be in DFU mode.
    From what I can see, the command was completed successfully.

    Did you use 'lsusb' to check for 'Analog Devices, Inc. USB download gadget'?
    If you can see it continue with the instructions for flashing with DFU utils.

    Dumitru

  • Thanks Dumitru, I checked the following things (and some steps from the DFU guide) but still can't seem to get it in the right mode it needs to be in:

    • an `lsusb` was performed after each step before and after `xsct`.  The only times a new USB device was detected was when the JTAG-HS3 and (optionally) the UARTJTAG was plugged in.  The name "Analog Devices" was not found, nor was the VID 0456.
    • `iio_attr -a -C fw_version` printed `No IIO context found.`
    • `sudo dfu-util --list` shows nothing listed (tried a few times)
    • Tried with and without unplugging the 10-pin JTAG cable from the Pluto after the `xsct` process
    • Tried with and without opening the UARTJTAG serial port (not the Pluto on-board FTDI on the right USB socket)
    • Tried pressing the device button with a toothpick after
    • Tried the Pluto USB port that I normally try on the left ("P2"), as well as the port on the right ("P3")
    • No new mass storage devices appeared at any time
    • The LEDs showed the same each time.  The left LED ("DS2") lights dimly, while the right LED ("DS1") remains off.

    Paul

  • Did you test this with 'JTAG BOOT' jumper on the UARTJTAG plugged in?

    You should see some output on the UART from the ADALM-UARTJTAG usb port when power-cycling the Pluto if the device boots into DFU. 

    U-Boot PlutoSDR v0.20-PlutoSDR-00066-g90401ce9ce (Nov 17 2023 - 10:28:18 +0100)
    
    I2C:   ready
    DRAM:  ECC disabled 512 MiB
    SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB
    In:    serial@e0001000
    Out:   serial@e0001000
    Err:   serial@e0001000
    Model: Zynq Pluto SDR Board
    Hit any key to stop autoboot:  0 
    Booting silently
    BOOT failed entering DFU mode ...
    SF: Locked
    gpio: pin 15 (gpio 15) value is 1
    Entering DFU SF mode ...