KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
Hello,
I have Pluto Rev B device and updated it in DFU mode by running uboot-env.dfu from plutosdr-fw-v0.38.zip
update.bat uboot-env.dfu
that was my mistake.
Then I run: update.bat pluto.dfu
which worked well and I got to firmware version 0.38 .
Now I need to move back to my old version 0.32 custom build firmware.
I tried copying plutosdr-fw-v0.32/pluto.frm to the USB mass storage and tried to do the same in DFU mode by running
update.bat plutosdr-fw-v0.38/pluto.dfu
and that doesn't work.
My questions:
Does Pluto support downgrading from form version 0.38 to 0.32?
What update.bat uboot-env.dfu does to Pluto? does it change uboot-env in a way that pluto.frm or pluto.dfu can't override?
How can I move back to version 0.32 version from version 0.38?
Thank you
Hello,
If you want to go back to V0.32 you can do the steps for update with the files of that release found here
Best regards!
Sorry, but that doesn't work.
When I turn on and log in to the Pluto board it shows me
Welcome to:
______ _ _ _________________
| ___ \ | | | / ___| _ \ ___ \
| |_/ / |_ _| |_ ___ \ `--.| | | | |_/ /
| __/| | | | | __/ _ \ `--. \ | | | /
| | | | |_| | || (_) /\__/ / |/ /| |\ \
\_| |_|\__,_|\__\___/\____/|___/ \_| \_|
v0.38
Then I copy the 0.32 firmware plutosdr-fw-v0.32/pluto.frm to the USB mass storage device and Eject the mass storage.
It starts blinking very fast and completed the "update". Then I unplug and plug back in the board and it doesn't event come up in the Windows Device Manager tree adn it doesn't come up as a mass storage device.
So I have to push the DFU button and switch to DFU mode and run
UPDATE.BAT plutosdr-fw-v0.38/pluto.dfu
to go back to v0.38. Basically the downgrading from 0.38 to 0.32 doesn't work.
If you copy all the content from v0.32 archive inside mass storage pluto then eject you it should work.
Make sure you don't have files from v0.38 inside mass storage pluto just the ones from v0.32
Thank you Ionut. That worked. Can you please explain to me what's the difference between pluto.frm and pluto.dfu ?
As I understand pluto.frm is the firmware for USB mass storage device update and pluto.dfu is the firmware update image from DFU mode. They both write the same Pluto image. Why are they different files?
Thank you
Thank you Ionut. That worked. Can you please explain to me what's the difference between pluto.frm and pluto.dfu ?
As I understand pluto.frm is the firmware for USB mass storage device update and pluto.dfu is the firmware update image from DFU mode. They both write the same Pluto image. Why are they different files?
Thank you
They both write the same Pluto image. Why are they different files?
DFU requires a dedicated file header and format. The FRM has also additional information and that wouldn't work for DFU.