Post Go back to editing

Pluto doesn't work after a firmware update

Category: Software

Hello,

I have Pluto Rev B device and updated it in DFU mode by running uboot-env.dfu from plutosdr-fw-v0.38.zip 

update.bat uboot-env.dfu

that was my mistake.

Then I run: update.bat pluto.dfu 

which worked well and I got to firmware version 0.38 .

Now I need to move back to my old version 0.32 custom build firmware.

I tried copying plutosdr-fw-v0.32/pluto.frm to the USB mass storage and tried to do the same in DFU mode by running

update.bat plutosdr-fw-v0.38/pluto.dfu

and that doesn't work.

My questions:

Does Pluto support downgrading from form version 0.38 to 0.32?

What update.bat uboot-env.dfu does to Pluto? does it change uboot-env in a way that pluto.frm or pluto.dfu can't override?

How can I move back to version 0.32 version from version 0.38?

Thank you

Edit Notes

typos and restructuring of my questions
[edited by: Cristian.B. at 7:57 AM (GMT -4) on 6 Apr 2024]
Parents
  • Hello, 
    If you want to go back to V0.32 you can do the steps for update with the files of that release found here 

    Best regards!

  • Sorry, but that doesn't work.

    When I turn on and log in to the Pluto board it shows me 

    Welcome to:
    ______ _ _ _________________
    | ___ \ | | | / ___| _ \ ___ \
    | |_/ / |_ _| |_ ___ \ `--.| | | | |_/ /
    | __/| | | | | __/ _ \ `--. \ | | | /
    | | | | |_| | || (_) /\__/ / |/ /| |\ \
    \_| |_|\__,_|\__\___/\____/|___/ \_| \_|

    v0.38

    Then I copy the 0.32 firmware plutosdr-fw-v0.32/pluto.frm to the USB mass storage device and Eject the mass storage.

    It starts blinking very fast and completed the "update". Then I unplug and plug back in the board and it doesn't event come up in the Windows Device Manager tree adn it doesn't come up as a mass storage device.

    So I have to push the DFU button and switch to DFU mode and run 

    UPDATE.BAT plutosdr-fw-v0.38/pluto.dfu

    to go back to v0.38. Basically the downgrading from 0.38 to 0.32 doesn't work.

Reply
  • Sorry, but that doesn't work.

    When I turn on and log in to the Pluto board it shows me 

    Welcome to:
    ______ _ _ _________________
    | ___ \ | | | / ___| _ \ ___ \
    | |_/ / |_ _| |_ ___ \ `--.| | | | |_/ /
    | __/| | | | | __/ _ \ `--. \ | | | /
    | | | | |_| | || (_) /\__/ / |/ /| |\ \
    \_| |_|\__,_|\__\___/\____/|___/ \_| \_|

    v0.38

    Then I copy the 0.32 firmware plutosdr-fw-v0.32/pluto.frm to the USB mass storage device and Eject the mass storage.

    It starts blinking very fast and completed the "update". Then I unplug and plug back in the board and it doesn't event come up in the Windows Device Manager tree adn it doesn't come up as a mass storage device.

    So I have to push the DFU button and switch to DFU mode and run 

    UPDATE.BAT plutosdr-fw-v0.38/pluto.dfu

    to go back to v0.38. Basically the downgrading from 0.38 to 0.32 doesn't work.

Children