Hi i need to realize a FMCW doppler estimation radar with one single Adalm-Pluto operating in full-duplex, programmed with Matlab. The estimation is always uncorrect but i don't know the reason because every time i try tu simulate without the Pluto SDR the estimation is correct. I tried also to separate the 2 antennas to remove the energy's dependence but the result are always wrong. How should i configure the device to resolve de problem? I am sure that the code about the digital elaboration is correct because when i try to simulate with an ideal ambient emulate with Matlab the estimation is correct