Post Go back to editing

Simple op-amps for the adalm1k, specifically the inverting configuration

Category: Hardware
Product Number: OP97
Software Version: PixelPulse2

Simple op-amps for the adalm1k, specifically the inverting configuration: See Fig. 1.4.

Firstly, I have to come clean -- I do not understand the relevance of the load resistor (10K) and the addition of a 2.5v supply in this particular circuit. (Athough it makes perfect sense in the preceding Buffer circuit) Does this have something to do with the fact that you cannot get a negative waveform on the Adalm1k as you do on the Adalm2k and, therefore, you need this to compensate in some way?

The lab begins with the source on CH-A as a sine wave set to 2.1 V Min value and a 2.9 V Max value (0.8 Vp-p centered on 2.5V.)

I got really inconsistent results using my AD8542 dual amp as a single op amp (because I did not have AD8541) so I substituted OP97

In the first part of the lab, we use a 4.7k as the negative feedback resistor. With that in place, I measured on CH-B a sine wave between 3.3v and 3.85v.

Then, we are asked to replace the 4.7k resistor with a 10k one where I measured 3.3v to 3.8 zero volts on CH-B, slightly lower than above.

According to the formula Vout = R f / R in * Vin so these results seem a bit low to me. I am wondering if that is because of voltage drop-outs.

Edit Notes

Added URL and swapped out AD8542 for OP97 Simplified the issues
[edited by: enjay at 11:18 AM (GMT -4) on 23 Jun 2023]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.