Post Go back to editing

UNABLE TO USE THE FMCOMM BLOCKS IN GNU RADIO 3.10.5

Category: Software
Product Number: SN:00981 S21-0549

I HAVE TRIED ALL POSSIBLE INSTALLATION PROCEDURES BUT STILL GETTING THE IIO ERROR CONSISTENTLY. I HAVE USED THE FOLLOWING LINK TO INSTALL DEPENDENCIES AND THEN INSTALLED GNU RADIO 3.10.5.

https://wiki.analog.com/resources/tools-software/linux-software/gnuradio#download_and_build_libiio

AFTER THE INSTALLATION I AM FACING THE FOLLOWING ERROR:

<<< Welcome to GNU Radio Companion 3.10.5.0 >>>

Block paths:
/usr/share/gnuradio/grc/blocks

Loading: "/home/cipl/tyest1.grc"
>>> Done

Generating: '/home/cipl/tyest1.py'

Executing: /usr/bin/python3 -u /home/cipl/tyest1.py

Traceback (most recent call last):
  File "/home/cipl/tyest1.py", line 169, in <module>
    main()
  File "/home/cipl/tyest1.py", line 147, in main
    tb = top_block_cls()
  File "/home/cipl/tyest1.py", line 99, in __init__
    self.iio_fmcomms2_source_0 = iio.fmcomms2_source_fc32('ip:192.168.1.173', [True, True, False, False], 32768)
AttributeError: module 'gnuradio.iio' has no attribute 'fmcomms2_source_fc32'

>>> Done (return code 1)

PLEASE HELP WITH THE INSTALLATION PROCESS .

THANK YOU

Parents
  • How did you install gnuradio ? Did you build it from source or via package manager ? What OS are you using ? Did you have an older version of gnuradio prior to 3.10.5 installed on this PC ?

  • Hi,

    I installed my GNURadio from this link ( https://wiki.gnuradio.org/index.php/InstallingGR ) for windows with Radioconda installer.

    I use Windows 10 64-bit version.

    I had previous version. I uninstalled it first than installed 3.10.5 version.

    My error is something like this:

                                                    line 199, in __init__
                                                    self.iio_pluto_source_0 = iio.fmcomms2_source_fc32('local:' if 'local:' else iio.get_pluto_uri(), [True, True], 32768)
                                                    AttributeError: module 'gnuradio.iio' has no attribute 'fmcomms2_source_fc32'

    Thanks for support.

    Best Regards,

    Bora Kilerci

  • Hi again,

    I deleted anything related about GNURadio and installed 3.10.4 again via Radioconda.

    It works, however TX and RX doesn't work simultaneously.

    I created a fm receiver, works fine.

    Then created and transmitter, works fine.

    However, not at the same time. Error code under below

    File "D:\Yazilim\Amator_telsiz\SDR\GNU_Radio\Radar.py", line 212, in __init__ 

    self.iio_pluto_sink_0 = iio.fmcomms2_sink_fc32('' if '' else iio.get_pluto_uri(), [True, True], 32768, False)  #  I tried any methode, ip:192.168.2.1.local etc. nothing works when

    both tx and rx need to be work

    RuntimeError: No Pluto device found                =============>>>>>>>>      # I can work with other SDR softwares, like SDR Angel, SDR Console etc.

    OOOOOOOOOOOOO                                       =============>>>>>>>>     # The "counter" i would say when the code started by me it starts printing "O" 's in this line.

    QT GUI doesn't show up but code looks started

    I'm trying to make a basic Radar project.

    Thx for now.

    Best Regards,

    Bora Kilerci

Reply
  • Hi again,

    I deleted anything related about GNURadio and installed 3.10.4 again via Radioconda.

    It works, however TX and RX doesn't work simultaneously.

    I created a fm receiver, works fine.

    Then created and transmitter, works fine.

    However, not at the same time. Error code under below

    File "D:\Yazilim\Amator_telsiz\SDR\GNU_Radio\Radar.py", line 212, in __init__ 

    self.iio_pluto_sink_0 = iio.fmcomms2_sink_fc32('' if '' else iio.get_pluto_uri(), [True, True], 32768, False)  #  I tried any methode, ip:192.168.2.1.local etc. nothing works when

    both tx and rx need to be work

    RuntimeError: No Pluto device found                =============>>>>>>>>      # I can work with other SDR softwares, like SDR Angel, SDR Console etc.

    OOOOOOOOOOOOO                                       =============>>>>>>>>     # The "counter" i would say when the code started by me it starts printing "O" 's in this line.

    QT GUI doesn't show up but code looks started

    I'm trying to make a basic Radar project.

    Thx for now.

    Best Regards,

    Bora Kilerci

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.