Hi,
I'm working with Pluto using the FMComms2/3/4 source block on GNU Radio.
I found the following issue with the RX Gain settings behavior when Gain mode is set to Manual for both channels:
- When the flowchart is started the desired values for each RX Gain channel seems to be set correctly,
- If RX Gain for channel 1 is changed during runtime, it changes that for both channel 1 AND channel 2,
- If RX Gain for channel 2 is changed during runtime, it seems to do nothing at all.
I have tested this under Ubuntu 22.04 jammy as well under Windows 11 running GNU Radio using Radio Conda. Both versions of GNU Radio are 3.10.4.0.
Please find attached zip file containing the flowgraph that can be used check this behavior.
Kind Regards,
Deon