I set up the AD7920 12-bit ADC lab but do not get the screens that are shown. Here are my screens:





layout:


Why do I not get any output from the MISO logic analyzer ?
Could the chip layout be backwards from the web layout, as the "1" and "8" in the above picture are on the Right.
Thus, is this chip layout as:
top 5 6 7 8
bot: 4 3 2 1
whereas in the web instruction it is
top 8 7 6 5
bot 1 2 3 4
Also, where should I place the 1+ /1- leads of the oscilloscope to read the input voltage ?
I placed the 1+ at W1 and 1- at ground, but the oscilloscope shows zero voltage:

Thanks !