Post Go back to editing

FSK transmission using Adalm-Pluto SDR module

Thread Summary

The user seeks to transmit a simple FSK-modulated bit sequence using the Adalm-Pluto in MATLAB or Simulink. The support engineer suggests adapting the QPSK example from the TransceiverToolbox and recommends several books on receiver design. The user is also advised to explore MathWorks' file exchange and the GNU Radio community for additional FSK examples.
AI Generated Content

I would like to transmit the following bits: [1 0 0 1 1 0 1] using FSK modulation and the Adalm-Pluto as the transmitter and receiver. Would anyone know how to do this on matlab or Simulink?

I've looked at many examples on matlab, but they are all far too complex. 

Thanks,

A