Post Go back to editing

Transmitting a Continuous Wave (CW) signal using ADALM Pluto with GNU Radio

Thread Summary

The user wants to transmit a pure sine wave CW signal from ADALM Pluto using GNU Radio. The solution is to either send a purely real tone (zero out the I or Q signal) or generate I and Q tones that are in-phase. The user cannot bypass the mixer stages, so the output will be at LO + tone frequency. For Simulink users, the same principles apply, but specific guidance is needed for the Simulink setup.
AI Generated Content

I am currently working to transmit a Continuous Wave(CW) signal using ADALM Pluto with GNU Radio.  I want to transmit a simple CW signal out from the ADALM Pluto using the signal processing blocks in GNU Radio with only a single pure sine wave signal at the output of the ADALM Pluto transmitter.

As of now, the output of the ADALM Pluto transmitter I am getting is a complex signal(consists of a 0 degrees sine wave and a sine wave with 90 degrees out of phase) instead of a pure single sine wave at the Pluto transmitter's output. Is there a possible solution to transmit a CW signal of a single pure sine wave out from the ADALM Pluto using the signal processing blocks in GNU Radio?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.