Post Go back to editing

Adalm Pluto Burst Mode

Thread Summary

The user asked about the ADALM Pluto's burst mode sampling initiation and differences from normal mode. The final answer explains that burst mode sets the number of kernel buffers to 1, allowing for the largest contiguous buffer capture, while the FramesInBurst setting splits this buffer into smaller vectors on the host side. In normal mode, multiple buffers (4 by default) are used for continuous streaming without sample drops, provided data is pulled fast enough. The accompanying answer mentions that the question was moved to the Virtual Classroom for the ADI University Program.
AI Generated Content

Hi, 

I need to clarify that when does ADALM PLUTO start sampling in burst mode? Does it perform it when we initialize or call the sdrReceiver() method? What happens in between them? What is its difference from the normal operation mode? For example, does it perform the same thing when I set sdrReceiver.numFramesInBurst = 1 ? Also what else happens in between consecutive calls to sdrReceiver() method in burstMode? 

Thank you so much

Mert  

Parents Reply Children