KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
Hello,
I would like to test out the examples provided at this link:
https://github.com/analogdevicesinc/libiio/blob/master/examples/ad9361-iiostream.c
I would like to implement these examples in the ADALM-Pluto.
I have successfully been able to use "runme.sh" files mounted from a USB Flash Drive, but now I would like to try the C examples.
How can I do this in the ADALM-Pluto?
You can start using this example via libiio remote over IP network -
if you want to run it locally please see here:
https://www.gnuradio.org/assets/files/grcon2018/8-Michael_Hennerich.pdf
-Michael
Thank you,
So using the Examples in the Custom Applications Section, I would need to compile and run the exe on an external host that has a network route to the pluto?
In any case you link your application against libiio. If you do that on a remote PC, your application would create a network context or context from URI.
-Michael
Got it, I will check this out in detail.
In addition, What would be the best way to implement the libiio api for the ad936x from within the Pluto?
In other words, to be able to run the code with no external source. In this case, We would plug the Pluto into a power supply and the code would run automatically.
Please see my GRCon presentation it covers all this.
Please see my GRCon presentation it covers all this.