KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
Hello,
I would like to test out the examples provided at this link:
https://github.com/analogdevicesinc/libiio/blob/master/examples/ad9361-iiostream.c
I would like to implement these examples in the ADALM-Pluto.
I have successfully been able to use "runme.sh" files mounted from a USB Flash Drive, but now I would like to try the C examples.
How can I do this in the ADALM-Pluto?
You can start using this example via libiio remote over IP network -
if you want to run it locally please see here:
https://www.gnuradio.org/assets/files/grcon2018/8-Michael_Hennerich.pdf
-Michael
Thank you,
So using the Examples in the Custom Applications Section, I would need to compile and run the exe on an external host that has a network route to the pluto?
In any case you link your application against libiio. If you do that on a remote PC, your application would create a network context or context from URI.
-Michael
In any case you link your application against libiio. If you do that on a remote PC, your application would create a network context or context from URI.
-Michael
Got it, I will check this out in detail.
In addition, What would be the best way to implement the libiio api for the ad936x from within the Pluto?
In other words, to be able to run the code with no external source. In this case, We would plug the Pluto into a power supply and the code would run automatically.
Please see my GRCon presentation it covers all this.