• ADALM2000 Activity: Transformers

    Written By: Antoniu Miclaus Objective The objective of this activity is to investigate transformer characteristics in various configurations. Background AC Transformer Transformers only work…
  • Follow up to Which Transformers

    Follow up to Which Transformers. In a previous blog posted on July 11, 2014 I looked at a number of possible transformers to use with the Analog Discovery module that can be adapted to solder-less breadboards…
  • The Current Sense Transformer

    The Current Sense Transformer In past blogs we've discussed the current measurement features of the ADALM1000 (SMU). The ALM1000's SMU channels can measure DC currents from -200mA to +200mA. Because…
  • Which Transformers to use with Analog Discovery?

    Magnetic components ( i.e. inductors and transformers ) are important elements used in a wide range of electric and electronic applications such as power supplies, DC-DC converters, filters and RF circuits…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.