• ADALM2000 - Debugging SPI

    The objective of this tutorial is to use the Logic Analyzer instrument provided by the ADALM2000 (M2K) board and the Scopy software toolset to visualize SPI (Serial Peripheral Interface) transactions between…
  • ADALM2000 - How to Debug UART

    The objective of this tutorial is to use the Pattern Generator and Logic Analyzer instruments provided by the ADALM2000 (M2K) board and the Scopy software toolset to visualize UART (Universal Asynchronous…
  • ADALM2000 Activity: Build CMOS Logic Functions Using the CD4007 Array

    Written By: Doug Mercer and Antoniu Miclaus Objective The objective of this lab activity is to build the various CMOS logic functions possible with the CD4007 transistor array. The CD4007 contains…
  • ADALM2000 Activity: CMOS Logic Circuits, D-Type Latch

    Written By: Doug Mercer and Antoniu Miclaus Objective The objective of this lab activity is to reinforce the basic principles of CMOS logic from the previous lab activity titled “ ADALM2000 Activity…
  • ADALM2000 Activity: CMOS Logic Circuits, Transmission Gate XOR

    Written By: Antoniu Miclaus and Doug Mercer Objective The objective of this lab activity is to reinforce the basic principles of CMOS logic from the previous lab activity titled “ Build CMOS Logic…
  • ADALM2000 Activity: TTL Inverter and NAND Gate

    Written By: Antoniu Miclaus and Doug Mercer Objectives A variety of digital logic circuit techniques have been in use since the 1960s when integrated logic gates were first produced. In this laboratory…
  • Debug I2C with ADALM2000

    In this tutorial we will use ADALM2000 (M2K) board and the Logic Analyzer instrument provided by the Scopy software toolset to visualize I2C (Inter-Integrated Circuit) transactions between two devices…
  • Demonstrate PWM with flickering LEDs

    Demonstrate PWM with flickering LEDs. I recently purchased some flickering LED candles at the dollar store ( 2 for $1 ) to investigate the flickering LEDs. These LED candles came with a CR2032 3V coin…
  • Expanding the number of ADALM1000 digital inputs and outputs

    The ALM1000 has 4 general purpose digital input/output pins. What if you need more than 4 digital inputs/outputs? One solution is to use an 8-bit shift and store register like the CD4094 integrated circuit…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.