Post Go back to editing

ADQUADMXFE1EBZ MultiChip Sync

Category: Hardware
Product Number: ADQUADMXFE1EBZ

Hi All,

I'm actually working on the QuadMxFE Platform Rev.B with a custom FPGA design composed by a Petalinux Distribution and custom Software and custom firmware using the Xilinx JESD204 IP Core.

My goal is to achieve Phase determinism and allign 2 MxFEs. I already achieve the Phase determinism on 4 ADCs on the same chip however i have some difficulty to understand what is the workflow in order to achieve MCS. On the UG of AD9081 are explained many information about sysref sampling and correction on sample time, averaging etc... however i not identify clearly which parameters i need to monitor for MCS goal. 

Analyzing Analog Devices Linux distribution, I identify 3 main API routines issued by Matlab Code:

  • Stage1: OneShot Sync
  • Stage2: NCO Sync
  • Stage3: NCO Post Sync

I suppose that routine is enabled by the Matlab Code: "tx.setDeviceAttributeRAW('multichip_sync', '10', tx.iioDev3); %Issue MCS" and is executed until the phase bewteen SYSREF and LEMC is null. About this point, i monitor this parameter, however for every successive reading the value of the phase is different. Is that normal?If not which parameter i need to monitor?

Another question is about sysref mode of operation. The One shot procedure is executed using the averaged sysref, but is not any specification about the previous sysref operation mode. Until OneShot Sync the SYSREF is oneshot or continuous mode? I need to use both modes of operation of SYSREF? Maybe at startup oneshot and before running OneShot Sync enable continuous and averaging?

What about the sysref sampling indicator? In the UG seems like a very important point the Sampling Monitoring of the SYSREF in Monitor mode, however in your linux distribution and matlab code there is no point where this is executed.

Can you provide me a flow of the settings and parameters to monitor before and after running MCS?There is a priority order to monitor that? Thank you very much.

Best Regards,

Lucian.

  • Hi Lucian,

    Thank you for reaching out.

    A workflow that has achieved MCS on the Quad-MxFE Platform can be viewed in Figure 2 at the link below.

    https://www.analog.com/en/technical-articles/power-up-phase-determinism-using-multichip-synchronization.html

    Additional details regarding the MCS process can be viewed at the link below:

    https://wiki.analog.com/resources/eval/user-guides/quadmxfe/multichipsynchronization

    It sounds as though you are already familiar with some of the example MATLAB scripts for the platform given your comment above, but details on the example MATLAB script to achieve MCS is shown at the link below and is available in the QuadMxFE_MCS.m script available within the High-Speed Converter Toolbox:

    https://wiki.analog.com/resources/eval/user-guides/quadmxfe/quickbringup#quadmxfe_mcsm

    For the demonstrations we leverage the ADI JESD204C IP. Can you please confirm that you can achieve MCS on the platform using these existing example scripts? Will you plan to leverage the ADF4371 PLL as the clock source for the AD9081?

    https://wiki.analog.com/resources/eval/user-guides/quadmxfe/quick-start#software

    The example HDL Reference Design is shown in the link below:

    https://wiki.analog.com/resources/eval/user-guides/ad_quadmxfe1_ebz/ad_quadmxfe1_ebz_hdl

    All the Best,

    Mike

  • Hi Mike, 

    Maybe i was not too exaustive in my explanation.We are very familiar with the articles on the Wiki and also the reference designs that you send me, since we use that as example. However we actually working on a custom architecture different from your example as we are creating a custom board for a client.

    The syncronization and all your examples are ok with the VCU118 and Quad MxFE RevC however that is not what we need. 

    I'm actually working on the QuadMxFE Platform Rev.B with a custom FPGA design composed by a Petalinux Distribution and custom Software and custom firmware using the Xilinx JESD204 IP Core.

    The FPGA is different from VCU118 and all the architecture, FW, Software, HW is custom. We only use the Quad MxFE Rev.B as evaluation board. 

    My doubt was about specific signals issues and algorithm "stages", more specific and detailed of your Wiki articles. The general description of the algorithm is ok and i have no issues with that. 

    I've asking for a design workflow, is ok that is described in Figure 2:

    A workflow that has achieved MCS on the Quad-MxFE Platform can be viewed in Figure 2 at the link below.

    https://www.analog.com/en/technical-articles/power-up-phase-determinism-using-multichip-synchronization.html

    But we are not able to understand which API needs to be used in order to execute every stage. And also there are not specified which conditions need to be guaranteed or controlled at the end of at the beginning of the stages. 

    For example, as described in Figure 2 of your article, the MCS routine is executed until there is no Phase Slip between the SYSREF and LEMC.

    I suppose that routine is enabled by the Matlab Code: "tx.setDeviceAttributeRAW('multichip_sync', '10', tx.iioDev3); %Issue MCS" and is executed until the phase bewteen SYSREF and LEMC is null.

    Strobbing and reading the register 0x00B5 and 0x00B6 (i use also the API to read that) for each update and reading (successive) the SYSREF-LEMC phase is variable. Is that a normal? I think NO, but i not have any article or wiki document that explain that. On the UG is not specified how this phase is. I'm expecting that phase value remains constant when i reading it maybe 2-3 times. Maximum i'm expecting a little variation in DAC clock cycles but i reading variation like 1000,2000 DAC clocks for each time i strobe that registers. 

    When using One SHOT SYSREF, in the registers 0x0FB7, 0x0FB8  the value that i'm reading is related to the first time when SYSREF was sampled or is updated every time? If this registers are updated every time, when the sysref is off, what i read in those registers? 

    Can you provide a response at this questions? i'm not able to find any low level descripted workflow to use as reference. The Wiki articles are ok but the discription is high level and too generic. 

    Thank you.

    -Lucian.