Post Go back to editing

ADAR1000EVAL1Z CSB Selection

Category: Software

Hi,

As per Stingray board configuration , there are two switches( CSB ) to select the ADAR 1000 Chip configuration.

Since the switches are manually controlled. Is there any way to control them through programming.

Also what is the max clock rate of SPI in  stingray board



added tags
[edited by: stetz at 1:23 PM (GMT -4) on 14 Jul 2022]
Parents Reply
  • Hi,

    By connecting the CSB 3 and CSB 4 of one stingray board with the other, can I control all the parameters of 2 stingray boards.

    Also is there any ICD available explaining type of signals and their voltage levels for each signals for the stingray board.

    What is the maximum power  consumption of the stingray board at 12 V

Children