Post Go back to editing

Estimating Stingray(ADAR1000-EVAL1Z) power consumption

Category: Datasheet/Specs
Product Number: ADAR1000EVAL1Z

Hello,

I wonder the power consumption of Stingray for Tx state and Rx state

Thank you for your help.

Jaemin Kim



updated category
[edited by: sringwoo at 11:18 AM (GMT -4) on 20 Jul 2022]
  • Hi Jaemin, 

    In Tx state at nominal bias and all devices activated, the board is expected to consume approximately 70 W of DC power. In Rx state at nominal bias and all devices activated, the board is expected to consume approximately 20 W of DC power. Majority of the power consumption is due to the ADAR1000 (qty 8) and ADTR1107 (qty 32) ICs. Stingray (ADAR1000EVAL1Z) is powered from a single 12V rail with DC converters stepping down to the proper voltage rails for the various ICs. The converters/regulators have some inefficiencies which also contribute to the DC power consumption. A schematic can be found on the wiki if you want to see which components are used. 

    Sam