Post Go back to editing

Eval-AD4080-FMC Connection Issue

Hello,

I've connected the eval-AD4080-FMC board to Zedboard. I also inserted the SD card (which came with the AD4080 evaluation board) into the zedboard. Connected 50-ohm termination to the "INM" SMA input connector and a single-ended input signal to the "INP" SMA input connector.

After powering up, the ACE software displayed the eval-AD4080-FMC board in the associated hardware window. After selecting the board, it is unable to connect.

I've provided the AppTrace.log file.

  

2161.AppTrace.log

8400.ACE-AD4080.zip

Thank you,

Rushikesh

Edit Notes

Tag list updated
[edited by: RSD at 10:30 AM (GMT -5) on 18 Dec 2024]

Thread Notes

Parents
  • I had an issue getting everything running out of the box. It turns out that the jumper P10 on the AD4080 eval board was not shorted. As soon as I changed that, everything started talking to the ACE software. Before that, it would know that the board was there, but was not able to talk to it. It doesn't seem to be the same problem as you, because your photo shows P10 shorted.

Reply
  • I had an issue getting everything running out of the box. It turns out that the jumper P10 on the AD4080 eval board was not shorted. As soon as I changed that, everything started talking to the ACE software. Before that, it would know that the board was there, but was not able to talk to it. It doesn't seem to be the same problem as you, because your photo shows P10 shorted.

Children
No Data