Post Go back to editing

Eval-AD4080-FMC Connection Issue

Hello,

I've connected the eval-AD4080-FMC board to Zedboard. I also inserted the SD card (which came with the AD4080 evaluation board) into the zedboard. Connected 50-ohm termination to the "INM" SMA input connector and a single-ended input signal to the "INP" SMA input connector.

After powering up, the ACE software displayed the eval-AD4080-FMC board in the associated hardware window. After selecting the board, it is unable to connect.

I've provided the AppTrace.log file.

  

2161.AppTrace.log

8400.ACE-AD4080.zip

Thank you,

Rushikesh

Edit Notes

Tag list updated
[edited by: RSD at 10:30 AM (GMT -5) on 18 Dec 2024]

Thread Notes

Parents
  • I have a very similar issue. ACE (1.30.3323.1470) recognizes the AD4080/Zed board.  However, in the AD4080Board page, it indicates "Unsupported Linux version".  I have installed ADI-Kuiper-for-Evaluation-2024-08-27.img on a different SD card, but no change.

    When I attempt to capture data, I get the message "ACE currently requires Hardware for Data Capture!".

    Any suggestions?

  • I was able to get the Eval-AD4080 talking to ACE on a different computer, but only after a Windows update and (apparently) swapping my USB cables.

    The original computer seems to not recognize the Eval-AD4080 in any way..

  • Hi,

    Can you please confirm a couple of points for me to help debug your issue better --

    1. You are running ACE (x64) and not ACE (x86) -- unfortunately the IIO hardware module is not supported in the x86 application. You can check which version you're running through the application's title bar -- you should be seeing (x64) after the version number. 



      If the (x64) is not present on the title bar, please make sure you're opening ACE from the location C:\Program Files\Analog Devices\ACE

    2. The EVAL-AD4080 board is being detected and displayed as a tile in the Attached Hardware section of ACE. Here is an example of what it looks like when a controller is detected. I've just used a different board here.
    3. You have the ACE IIO Components suite installed. The installer can be found here: C:\Program Files (x86)\Analog Devices\ACE\AceIIOComponents.exe. Please check all the components when running the installer.

    If all those steps seem good to you, please attach the AppTrace.log file here to help us debug further. Please follow these steps:

    1. Open ACE with your hardware connected and powered on.
    2. Click on the "Refresh Attached Hardware" tile.
    3. Wait 5 seconds.
    4. Click the "Refresh Attached Hardware" tile once more.
    5. Wait 5 seconds.
    6. Use the dropdown at the top right corner of the application -> Show Log File
    7. Save the file in a convenient location and attach it to a response here.

    Hope that helps.

    Thanks,
    Sid

Reply
  • Hi,

    Can you please confirm a couple of points for me to help debug your issue better --

    1. You are running ACE (x64) and not ACE (x86) -- unfortunately the IIO hardware module is not supported in the x86 application. You can check which version you're running through the application's title bar -- you should be seeing (x64) after the version number. 



      If the (x64) is not present on the title bar, please make sure you're opening ACE from the location C:\Program Files\Analog Devices\ACE

    2. The EVAL-AD4080 board is being detected and displayed as a tile in the Attached Hardware section of ACE. Here is an example of what it looks like when a controller is detected. I've just used a different board here.
    3. You have the ACE IIO Components suite installed. The installer can be found here: C:\Program Files (x86)\Analog Devices\ACE\AceIIOComponents.exe. Please check all the components when running the installer.

    If all those steps seem good to you, please attach the AppTrace.log file here to help us debug further. Please follow these steps:

    1. Open ACE with your hardware connected and powered on.
    2. Click on the "Refresh Attached Hardware" tile.
    3. Wait 5 seconds.
    4. Click the "Refresh Attached Hardware" tile once more.
    5. Wait 5 seconds.
    6. Use the dropdown at the top right corner of the application -> Show Log File
    7. Save the file in a convenient location and attach it to a response here.

    Hope that helps.

    Thanks,
    Sid

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.