Hello,
I've connected the eval-AD4080-FMC board to Zedboard. I also inserted the SD card (which came with the AD4080 evaluation board) into the zedboard. Connected 50-ohm termination to the "INM" SMA input connector and a single-ended input signal to the "INP" SMA input connector.
After powering up, the ACE software displayed the eval-AD4080-FMC board in the associated hardware window. After selecting the board, it is unable to connect.
I've provided the AppTrace.log file.

Thank you,
Rushikesh
Edit Notes
Tag list updated[edited by: RSD at 10:30 AM (GMT -5) on 18 Dec 2024]