Post Go back to editing

Eval-AD4080-FMC Connection Issue

Hello,

I've connected the eval-AD4080-FMC board to Zedboard. I also inserted the SD card (which came with the AD4080 evaluation board) into the zedboard. Connected 50-ohm termination to the "INM" SMA input connector and a single-ended input signal to the "INP" SMA input connector.

After powering up, the ACE software displayed the eval-AD4080-FMC board in the associated hardware window. After selecting the board, it is unable to connect.

I've provided the AppTrace.log file.

  

2161.AppTrace.log

8400.ACE-AD4080.zip

Thank you,

Rushikesh

Edit Notes

Tag list updated
[edited by: RSD at 10:30 AM (GMT -5) on 18 Dec 2024]

Thread Notes

Parents Reply Children
  • Hi,

    Apologies to you both for the lack of follow up on this thread, we did not receive notification of it initially as it was originally posted in another forum and then moved to the ACE forum, as such our support team only received notifications when the replies were posted.

     glad you were able to resolve the issue, please let us know if you have any further issues with this.

    Thanks,
    Eoin