Post Go back to editing

Eval-AD4080-FMC Connection Issue

Hello,

I've connected the eval-AD4080-FMC board to Zedboard. I also inserted the SD card (which came with the AD4080 evaluation board) into the zedboard. Connected 50-ohm termination to the "INM" SMA input connector and a single-ended input signal to the "INP" SMA input connector.

After powering up, the ACE software displayed the eval-AD4080-FMC board in the associated hardware window. After selecting the board, it is unable to connect.

I've provided the AppTrace.log file.

  

2161.AppTrace.log

8400.ACE-AD4080.zip

Thank you,

Rushikesh

Edit Notes

Tag list updated
[edited by: RSD at 10:30 AM (GMT -5) on 18 Dec 2024]

Thread Notes

Parents Reply Children