Controlling the setup of ADS9+AD9081 with two Computers that defer by the Windows 10-11 environment
The setup functions properly when controlled by another Windows 10 computer and fails when using the Windows 11 computer.
Both running the same version of ACE.
(Clarify: The main difference between the two computers is that the one experiencing issues running Windows11, while the functioning one is on Windows10.)