Post Go back to editing

Import csv file to ACE ADF4377 eval

Category: Software
Product Number: ADF4377 Board
Software Version: ACE 1.28.3252.1429

While monitoring the memory map, whenever I import a .csv configuration a window pops up indicating File successfully imported and I can see the values in the memory map updated. However when I click the 'OK' button the memory map reverts to the previous values and the imported values are lost.

I should also mention then when I move the mouse pointer within the pop-up that says 'File Successfully Imported' the pointer changes in to a circulating timer as if the program is still busy. I move this over the OK button and press.. the pop-up closes and the values in the memory map revert to previous.

Is this a bug or do I need to change a setting somewhere?

Thanks for any help!