ACE 1.26.3240.1417 installed (offline version) but fails to open
below screen appears upon opening later to this it vanishes
Installation went on successfully, installed on PC with OS Windows 10Pro, with 16 GB RAM
ACE 1.26.3240.1417 installed (offline version) but fails to open
below screen appears upon opening later to this it vanishes
Installation went on successfully, installed on PC with OS Windows 10Pro, with 16 GB RAM
Hi,
Can you check if there was a log file generated for the app startup, I can't reproduce the issue to investigate on my side. It should be in the AppData folder on your machine, see path example below:
C:\Users\USERNAME\AppData\Local\Analog Devices\ACE\AppTrace.log
If you can send the file or even the error messages it would help see if there is something missing.
16:34:15 Logging Started - 7/11/2022 4:34:15 PM 16:34:15 Analysis | Control | Evaluation 1.26.3240.1417 16:34:15 Using .NET Framework 4.8.4250.0 16:34:15 Loading from path C:\Program Files\Analog Devices\ACE\ACE.exe 16:34:15 Checking command line for DEBUGFROM option... 16:34:15 - Debugging path is 16:34:36 Assembly AnalogDevices.Csa.UI.Rad.dll cannot be authenticated. PartialChain: A certificate chain could not be built to a trusted root authority. 16:34:36 Assembly AnalogDevices.Csa.App.DataInstallers.dll cannot be authenticated. PartialChain: A certificate chain could not be built to a trusted root authority. 16:34:36 Assembly AnalogDevices.Csa.App.DeviceApiInstallers.dll cannot be authenticated. PartialChain: A certificate chain could not be built to a trusted root authority. 16:34:36 Assembly AnalogDevices.Csa.App.Installers.dll cannot be authenticated. PartialChain: A certificate chain could not be built to a trusted root authority. 16:34:36 Assembly AnalogDevices.Csa.VectorGenerator.UI.dll cannot be authenticated. PartialChain: A certificate chain could not be built to a trusted root authority. 16:34:36 AceCore is setting environment variables 16:34:36 AceCore is setting required default culture 16:34:36 AceCore is initializing the IOC container 16:34:37 AceCore is adding facilities 16:34:37 AceCore is registering components 16:34:37 Error registering ACE core components: Castle.MicroKernel.Resolvers.DependencyResolverException: Missing dependency. Component AnalogDevices.Csa.CastleSupport.Plugins.Extensions.WindsorExtensionPointManager has a dependency on AnalogDevices.Csa.Interfaces.IXElementInfo, which could not be resolved. Make sure the dependency is correctly registered in the container as a service, or provided as inline argument. ---> Castle.MicroKernel.Handlers.HandlerException: Handler for AnalogDevices.Csa.Interfaces.IXElementInfo was not found. at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.TryGetHandlerFromKernel(DependencyModel dependency, CreationContext context) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.ResolveFromKernelByType(CreationContext context, ComponentModel model, DependencyModel dependency) --- End of inner exception stack trace --- at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.ResolveFromKernelByType(CreationContext context, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.Facilities.Startable.StartFlag.StartAll() at System.EventHandler.Invoke(Object sender, EventArgs e) at Castle.MicroKernel.DefaultKernel.OptimizeDependencyResolutionDisposable.Dispose() at Castle.Windsor.WindsorContainer.Install(IWindsorInstaller[] installers) at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents(IEnumerable`1 installers) 16:34:37 System.InvalidOperationException: Error registering ACE core components: Missing dependency. Component AnalogDevices.Csa.CastleSupport.Plugins.Extensions.WindsorExtensionPointManager has a dependency on AnalogDevices.Csa.Interfaces.IXElementInfo, which could not be resolved. Make sure the dependency is correctly registered in the container as a service, or provided as inline argument. ---> Castle.MicroKernel.Resolvers.DependencyResolverException: Missing dependency. Component AnalogDevices.Csa.CastleSupport.Plugins.Extensions.WindsorExtensionPointManager has a dependency on AnalogDevices.Csa.Interfaces.IXElementInfo, which could not be resolved. Make sure the dependency is correctly registered in the container as a service, or provided as inline argument. ---> Castle.MicroKernel.Handlers.HandlerException: Handler for AnalogDevices.Csa.Interfaces.IXElementInfo was not found. at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.TryGetHandlerFromKernel(DependencyModel dependency, CreationContext context) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.ResolveFromKernelByType(CreationContext context, ComponentModel model, DependencyModel dependency) --- End of inner exception stack trace --- at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.ResolveFromKernelByType(CreationContext context, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.Facilities.Startable.StartFlag.StartAll() at System.EventHandler.Invoke(Object sender, EventArgs e) at Castle.MicroKernel.DefaultKernel.OptimizeDependencyResolutionDisposable.Dispose() at Castle.Windsor.WindsorContainer.Install(IWindsorInstaller[] installers) at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents(IEnumerable`1 installers) --- End of inner exception stack trace --- at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents(IEnumerable`1 installers) at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents() at AnalogDevices.Csa.App.Installers.Ace.AceCore.Initialize() 16:34:37 Unhandled application exception: System.InvalidOperationException: Error registering ACE core components: Missing dependency. Component AnalogDevices.Csa.CastleSupport.Plugins.Extensions.WindsorExtensionPointManager has a dependency on AnalogDevices.Csa.Interfaces.IXElementInfo, which could not be resolved. Make sure the dependency is correctly registered in the container as a service, or provided as inline argument. ---> Castle.MicroKernel.Resolvers.DependencyResolverException: Missing dependency. Component AnalogDevices.Csa.CastleSupport.Plugins.Extensions.WindsorExtensionPointManager has a dependency on AnalogDevices.Csa.Interfaces.IXElementInfo, which could not be resolved. Make sure the dependency is correctly registered in the container as a service, or provided as inline argument. ---> Castle.MicroKernel.Handlers.HandlerException: Handler for AnalogDevices.Csa.Interfaces.IXElementInfo was not found. at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.TryGetHandlerFromKernel(DependencyModel dependency, CreationContext context) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.ResolveFromKernelByType(CreationContext context, ComponentModel model, DependencyModel dependency) --- End of inner exception stack trace --- at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.ResolveFromKernelByType(CreationContext context, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.MicroKernel.Resolvers.DefaultDependencyResolver.Resolve(CreationContext context, ISubDependencyResolver contextHandlerResolver, ComponentModel model, DependencyModel dependency) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.CreateConstructorArguments(ConstructorCandidate constructor, CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.Instantiate(CreationContext context) at Castle.MicroKernel.ComponentActivator.DefaultComponentActivator.InternalCreate(CreationContext context) at Castle.MicroKernel.ComponentActivator.AbstractComponentActivator.Create(CreationContext context, Burden burden) at Castle.MicroKernel.Lifestyle.AbstractLifestyleManager.CreateInstance(CreationContext context, Boolean trackedExternally) at Castle.MicroKernel.Lifestyle.SingletonLifestyleManager.Resolve(CreationContext context, IReleasePolicy releasePolicy) at Castle.MicroKernel.Handlers.DefaultHandler.ResolveCore(CreationContext context, Boolean requiresDecommission, Boolean instanceRequired, Burden& burden) at Castle.MicroKernel.Handlers.DefaultHandler.Resolve(CreationContext context, Boolean instanceRequired) at Castle.Facilities.Startable.StartFlag.StartAll() at System.EventHandler.Invoke(Object sender, EventArgs e) at Castle.MicroKernel.DefaultKernel.OptimizeDependencyResolutionDisposable.Dispose() at Castle.Windsor.WindsorContainer.Install(IWindsorInstaller[] installers) at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents(IEnumerable`1 installers) --- End of inner exception stack trace --- at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents(IEnumerable`1 installers) at AnalogDevices.Csa.App.Installers.Ace.AceCore.RegisterComponents() at AnalogDevices.Csa.App.Installers.Ace.AceCore.Initialize() at AnalogDevices.Csa.App.Installers.Ace.AceCore.Resolve[T](String componentId) at AnalogDevices.Csa.App.Wpf.CsaApplication.OnStartup(StartupEventArgs args) at System.Windows.Application.<.ctor>b__1_0(Object unused) at System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs) at System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler) at System.Windows.Threading.DispatcherOperation.InvokeImpl() at MS.Internal.CulturePreservingExecutionContext.CallbackWrapper(Object obj) at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state, Boolean preserveSyncCtx) at System.Threading.ExecutionContext.Run(ExecutionContext executionContext, ContextCallback callback, Object state, Boolean preserveSyncCtx) at System.Threading.ExecutionContext.Run(ExecutionContext executionContext, ContextCallback callback, Object state) at MS.Internal.CulturePreservingExecutionContext.Run(CulturePreservingExecutionContext executionContext, ContextCallback callback, Object state) at System.Windows.Threading.DispatcherOperation.Invoke() at System.Windows.Threading.Dispatcher.ProcessQueue() at System.Windows.Threading.Dispatcher.WndProcHook(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam, Boolean& handled) at MS.Win32.HwndWrapper.WndProc(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam, Boolean& handled) at MS.Win32.HwndSubclass.DispatcherCallbackOperation(Object o) at System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs) at System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler) at System.Windows.Threading.Dispatcher.LegacyInvokeImpl(DispatcherPriority priority, TimeSpan timeout, Delegate method, Object args, Int32 numArgs) at MS.Win32.HwndSubclass.SubclassWndProc(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam) at MS.Win32.UnsafeNativeMethods.DispatchMessage(MSG& msg) at System.Windows.Threading.Dispatcher.PushFrameImpl(DispatcherFrame frame) at System.Windows.Application.RunDispatcher(Object ignore) at System.Windows.Application.RunInternal(Window window) at AnalogDevices.Csa.App.Wpf.Program.Main() 16:34:37 Logging Stopped - 7/11/2022 4:34:37 PM 16:34:37 Application RunDuration = 0:00:00:22.9520816 16:34:37 Application PeakPhysicalMemory = 103,243,776 16:34:37 Application PeakVirtualMemory = 5,189,685,248 16:34:37 UsageLogger cannot log because IUsageLoggingProvider isn't defined
apptarce log file attached
These lines could indicate an issue if your machine is unable to chain the certs -
16:34:36 Assembly AnalogDevices.Csa.App.DataInstallers.dll cannot be authenticated.
PartialChain: A certificate chain could not be built to a trusted root authority.
This could indicate your machine in use has out of date root certificates. You can check online, but if this is the case you can likely get around this by getting the latest Windows updates or manually updating the root certs on your machine.
The other potential issue I'm seeing here is this:
16:34:37 System.InvalidOperationException: Error registering ACE core components: Missing dependency.
Could you send a screenshot or even just a text list of the plug-ins that have been installed with your offline installers. It will help us confirm whether there is an issue with required offline dependencies or if we should check the certificates issues.
They should be in this location: C:\ProgramData\Analog Devices\ACE\Plugins
a) First suggestion need some time time to check.
b) Folder Plugins does not exist in the ACE folder
We'll have to investigate that further, if that directory is missing that means you will not have all required dependencies.
Are you able to connect to the internet temporarily on this machine to use the web installer? That should pull packages from the package feed.
No. there is no provision to connect the PC to internet.
Can i manually add packages??
You could use the "minimal" ACE installer released with v1.26 to install the application with only the "core" dependencies on another machine. If you already have ACE you can scrub the installation to only get the core plug-ins when you install the minimal version. Details can be found in this article: wiki.analog.com/.../installscrub
After you have it installed, you can zip the contents of the C:\ProgramData\Analog Devices\ACE\Plugins directory you could move them to your offline PC. This will only have the bare minimum requirements to launch ACE. Do you also have an ACEZIP for the product plug-in you are using to install it in offline mode?
Will try the above one.
For quicker job can u provide me link to older versions. as long its able to program ADMV8526 tunable filter i am fine with any version of software.
We do have some of our more recent releases on a page in the wiki linked above, however I don't think the offline installer links are included. I'll add a ticket to see if we can update the page to include offline installers for previous builds.
I have exactly the same problem on an (airgapped) Windows 7 SP1 x64 system.
The missing dependency on AnalogDevices.Csa.Interfaces.IXElementInfo is not a problem?
The problem occurs both with the minimal and the offline installers. I was able to install Board.AD971x.1.2019.44300.acezip without any error message.