Post Go back to editing

How to Interface EVAL-AD2428WD1BZ A2B Master with STM32 Nucleo-L552ZE-Q Using I2S/TDM for Upstream Audio Capture?

Category: Hardware
Product Number: AD2428

Hello ADI Team,

I am currently learning Automotive Audio Bus (A2B) communication using the following hardware:

  • A2B Master: EVAL-AD2428WD1BZ
  • A2B Subordinate: EVAL-AD2428WG1BZ
  • Microcontroller: STM32 Nucleo-L552ZE-Q
  • Software: SigmaStudio+

My requirement is to capture audio received from the A2B subordinate at the A2B master and transfer it to an external STM32 controller. The STM32 will then send the received audio data to a PC through USB.
How should I connect the AD2428 master to the STM32 Nucleo-L552ZE-Q?
Which exact AD2428 pins should I use for upstream audio output?

Parents
  • I want to tap the audio which is comming from the master transceiver in upstream data and i did connections as below:

    Setup:
    - JP5 (BCLK), pin 5 -> STM32 SAI SCK
    - JP6 (SYNC), pin 6 -> STM32 SAI FS
    - JP10 (DTX0), pin 2 -> STM32 SAI SD
    - GND from the SigmaStudio/USBi  9-pin header -> STM32 GND
    - Existing shorting caps left in place on all three jumpers; STM32 SAI is configured purely as a slave receiver (high-impedance, not driving anything)
    - Currently reading via polling (HAL_SAI_Receive), 24-bit, 2-channel, I2S protocol

    Problem: I am receiving data (not silence, not a timeout), but it does not resemble the actual audio being played into the board - it comes through as noise.
    i attached the .bin and .wav files which are collected form PC via stm32 USB.

Reply
  • I want to tap the audio which is comming from the master transceiver in upstream data and i did connections as below:

    Setup:
    - JP5 (BCLK), pin 5 -> STM32 SAI SCK
    - JP6 (SYNC), pin 6 -> STM32 SAI FS
    - JP10 (DTX0), pin 2 -> STM32 SAI SD
    - GND from the SigmaStudio/USBi  9-pin header -> STM32 GND
    - Existing shorting caps left in place on all three jumpers; STM32 SAI is configured purely as a slave receiver (high-impedance, not driving anything)
    - Currently reading via polling (HAL_SAI_Receive), 24-bit, 2-channel, I2S protocol

    Problem: I am receiving data (not silence, not a timeout), but it does not resemble the actual audio being played into the board - it comes through as noise.
    i attached the .bin and .wav files which are collected form PC via stm32 USB.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.