AD2437
Production
The AD2437 A2B® transceiver provides a multichannel, I2S/TDM link over distances of up to 30 m between nodes. It embeds bidirectional synchronous pulse...
Datasheet
AD2437 on Analog.com
Hello,
I'am working on a high power AD2437 main and bus powered sub node.
When flashing with Sigma Studio + I got "Critical short found at main node" error message.
If I disable for the sub node the "enable two step discovery" option, the bus work fine.
I saw in another post that's due to A2B wire length incorrect.
I'am looking how to update the wire length in Sigma Studio +
Best regards
Loïc
I'm pretty sure in SS+ 2 step discovery expects a valid EEPROM for node ID on the next node. ADI boards come with that set, if you are using your own board then you need to do that.
As a general comment SS+ error messages are not helpful; for example if there was really a short then changing the discovery type would make no difference as a short is a short...YMMV
I'm pretty sure in SS+ 2 step discovery expects a valid EEPROM for node ID on the next node. ADI boards come with that set, if you are using your own board then you need to do that.
As a general comment SS+ error messages are not helpful; for example if there was really a short then changing the discovery type would make no difference as a short is a short...YMMV