Post Go back to editing

SigmaStudio plus cannot export config file for A2B analyzer studio

Thread Summary

The user encountered issues exporting A2B network configuration files from SigmaStudio+ and connecting to the A2B Bus Analyzer. The solution involved exporting the .dat file from SigmaStudio+, loading it into the A2B Analyzer Studio GUI, and starting the emulator. The user confirmed that the A2B bus analyzer is now working.
AI Generated Content
Category: Hardware
Product Number: A2B Bus Analyzer

Hi I am a new user for A2B Bus Analyzer and I found it's so hard to use. I have below questions and I cannot search any answer from internet.

Maybe my questions are so long and my English is so bad, but I really need some good man's help.

1. When I want to use A2B Bus Analyzer for simulate an A2B main node that it's must be need an configuration file generate by SigmaStudio.

   I tried nearly every version of SigmaStudio(2.2/2.3/2.4), all of them cannot export the system files. I did these steps:

   Draw a diagram like below:

 push the "Link Compile" button, and SW indicated "successful !". Then push the "Action" -> "Export System Files" -> choose the folder -> SW  indicated " successful " -> there is anything in the folder.

 I really have no idea about that.

2. I use SigmaStudio+ to download the project directly, but the SigmaStudio+ indicated below:

> A2B_0 :- A2B BUS Analyzer UI not Running/Installed
> A2B_0 :- Network Auto-configuration information saved successfully to DAT file
> A2B_0 :- Analyzer Detected in Network, Check if A2B BUS Analyzer UI is launched
> A2B_0 :- Unable to Connect to A2B Analyzer Device!
> A2B_0 :- Failed to trigger discovery!

But I the A2B analyzer studio is working at same time. (I'm using the A2B analyzer Stdio GUI because my seller staff told me that the older version is no longer supported.)