Hello,
I'm using SigmaStudio to set Main Node to TDM16. I'm sending 4 channels downstream from Main node (slots 0,1,2,3).
I have SlaveNode0 (PDM Mic) adding 1 channel.
So, the SlaveNode0 sends total of 5 channels downstream to SlaveNode2 (there is a SlaveNode1 which is just being used as a pass through node).
The SlaveNode2 is connected to ADAU1961 Codec which drives single ended Stereo Headphone output via Lineout output.
Now the question:
I would like to hear PDM mic audio from one channel and Main nodes Line in audio from other channel on Codec's Stereo headphone output at SlaveNode2.
If i configure the SlaveNode2 to TDM2 mode then i hear ONLY Stereo data from Line in of Main node --. Makes sense because Codec, by default uses TDM slots 0 and 1
If i configure the SlaveNode2's AD2433 transceiver to TDM8, then i'm able to hear PDM microphone data from one speaker channel and Main nodes' line input data from other speaker channel.
Does AD2433 on SlaveNode2 send 8 TDM channels to Codec? How does Codec select and map these to Left and Right Channels?
BTW, ADAU1961 seems to support upto TDM4 ( i don't see any mention of TDM8)
Thanks
Chirag