In our setup, it seems that the SPDIF transmitter is announcing 44.1 kHz in these status bits, even though the actual audio signal is 48 kHz.
The SPDIF transmitter must declare 48 kHz in the IEC-60958 channel status bits (bits 24–27).
Is there any way to configure or override the IEC-60958 channel status bits in A2B → SPDIF module so that they match the actual output sampling rate?
If so, could you indicate where this configuration is located (firmware option, SDK setting, register field, etc.)?