Post Go back to editing

Consuming 32 downstream/32 upstream

Thread Summary

The user inquired about using 32 Downstream/32 Upstream channels for a loopback test, considering bandwidth limitations as outlined in the AD242x_TRM. The final answer suggests using the latest Sigma Studio+ and A2BPlugin to simulate the system and verify if the configuration is feasible based on slot numbers, slot width, cable length, and number of nodes.
AI Generated Content
Category: Hardware
Product Number: AD2428

Hello

I would like to check if I can use 32 Downstream/32upstream channels to perform the same loopback test. I have read in the AD242x_TRM that there is bandwidth limitation and It is explained in a table (table 3.5) but also I can see in the section of the loopback test that the pattern used is 32 bits sending downstream/upstream. 

Regards