Post Go back to editing

Are there any solutions for generating a sync signal on a custom embedded Linux system with an SoC as I2S master and ALSA?

Category: Software
Product Number: AD2433
Software Version: A2B Software for Linux 19.4.4

I am working on a project in which the host processor of the A2B network is a custom platform with embedded Linux. This platform features an SoC, which is to act as an I2S master, and the AD2433 as an A2B master node. I am using a customized version of the a2b-adsp-sc589_mini-linux demo app for Linux. My problem is that I cannot find a way to reimplement the pal_audioOpen functions so that the PCM interface of the SoC is configured to send a continuous SYNC signal. This means that I cannot perform a successful discovery. Are there any established solutions for this type of problem?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.