Hello everyone,
I'm new on this platform and I hope you'll be able to help me.
Also, pretty new working with A2B, so my understanding it's really limited for the moment.
I'm working with EVAL-AD2428WD1BZ, AD2428WB1BZ, ADUSB2EBUZ and a custom PCB that has a AD2428W Transceiver on the board.
Idea is to have EVAL-AD2428WD1BZ as master, custom PCB as slave0 and AD2428WB1BZ as slave1.
I've followed the QuickStartGuide and managed to connect the hardware. Jumper configuration on EVAL-AD2428WD1BZ it's the one on the QuickStartGuide.
I can listen the audio source from slave1 on master.
Hardware Block Diagram:
SigmaStudio Configuration:
I have a couple of questions.
PROBLEM1: I keep getting this validation report error
Question1: How can I disable or enable PDM interfaces channels or any other interfaces on slave0? (I think that's why I'm keep getting Problem1, because of unused interfaces)
In the image below you can see that PDM0 is grey/inactive.
I don't have any mic on my custom PCB, slave0. I think there's a way to send the mic signal from slave1 to master
but I don't know how to enable PDM on slave1. If I'm not wrong, I should connect Tx1-Ch from Microphone to PDM Slave1.
It's needed any other config to send upstream the mic sound?
Question2: If I have understood correctly, the Audio Source from Slave1 arrives at Slave0 on BN/BP pins and sent out via AN/AP pins.
Shouldn't I see some data from the sound on DTX0/DTX1 on Slave0 ? I have configured register 0x42, TX0EN = 1.
With the oscilloscope, I see a wave signal on Slave0 DTX0 Pin but it doesn't matter if TX0EN it's 0 or 1.
Also, I'm unable to set RX0EN = 1.
Question3: There is some AD2428W enable flow ? I've read the datasheet but still can't figure it out.
Maybe, I2SConfigure Register > I2S Global Configure Register > I2S Rate Register ...
The thing that I would like to know is the correctness or not of my SigmaStudio setup.
If I missed to specify something please tell me.
Thanks!