I am using an EVAL-AD2428WD1BZ board. I have audio in through the 3.5mm input. Simple music input from my phone.
I have a configuration for Signal Studio 4.7 where the sound is mixed into the first 4 channels of the A2B (Numbered 0-3). That works fine.
However, I cannot figure out how to do one or both things listed below.
1. Mix the sound into the 5th channel of the A2B bus. I think the Eval board supports only 4 channels, so that would mean that instead of using channels 0-3 (4 first channels) I want to use channels 1-4 (so that the 5th channel is mixed in and the first channel is excluded).
In this way I would get the same sound in channels 1-5.
2. Have sound sent only to channel 5 of the A2B.
The goal is to have sound sent out on channel 5 of the A2B. I cannot figure out how to this in Signal Studi0 v4.7. I heard that it is possible to mix in the sound into channel 5 by using configuration in to Sigma Studio and downloading it to the DSP, but there is no intuitive way of doing this. Can O please get some support in doing this.Is there anywhere I can upload my current Configuration setup (the sigma stdio project file)?