AD2428
Recommended for New Designs
The Automotive Audio Bus (A2B®) provides a multichannel, I2S/TDM link over distances of up to 15 m between nodes. It
embeds bidirectional synchronous...
Datasheet
AD2428 on Analog.com
From the datasheet of AD2428, It is mentioned as 16 Subordinate nodes are supported.
HiRakhesh
Regards
arun
Hi Rakhesh
Yes, it's possible. As I mentioned, the slot size and the number of slots are important factors. If you need to use it for your above requirement, the upstream slot size needs to be adjusted with the reduced bit size to achieve the bandwidth utilized for all 16 nodes (considering the necessary cable length and 2 slots each from all nodes.)
The best way to calculate this is to create a schematic in SigmaStudio or SigmaStudio+ and calculate the bandwidth accordingly.