Post Go back to editing

Audio play from slave input to master output

Category: Hardware
Product Number: AD2433W

I have 2 evalkits ad2433wa1bz (master) and ad2433wb1z (slave)

i managed to get audio routing from master input to both outputs, and routing from slave input to slave output.
However, i can't manage to figure out how to play audio from slave input to master output. i am not even sure if it is possible to do this only via register configs, or i need to externally go through the i2s pins

  • Hi  

    Without detailed information about your complete setup and configurations, it's difficult to provide specific comments. However, could you check the configuration of  the stream settings correctly done between the main node and the subnode? The register settings itself is enough to route the i2s/tdm data from one node to another.