AD2437
Pre release
The AD2437 A2B® transceiver provides a multichannel, I2S/TDM link over distances of up to 30 m between nodes. It embeds bidirectional synchronous pulse...
Datasheet
AD2437 on Analog.com
Dear Experts,
I am trying to perform a basic operation with the EVAL-AD2437A1MZ and EVAL-AD2437B1MZ setup. In Sigma Studio +, I can configure the circuit and compile it without issues, but when I attempt to download, I encounter the error "Main running interrupt not detected," preventing me from testing any operations.
Since the sub-node is BusPowered, I have set the jumper on JP4 on the main node board to the "MAIN" position. Are there any additional steps I need to take?
Additionally, I have reviewed the settings in Sigma Studio + based on advice in the following post, but instead of resolving the issue, I encounter different errors that don’t seem applicable to my case:
https://ez.analog.com/a2b/f/q-a/584262/sigma-studio-main-running-interrupt-not-detected
The setup I am attempting to operate is as follows:
[PC] - [USBi] - [EVAL-AD2437A1MZ] - [EVAL-AD2437B1MZ]
(USBi and EVAL-AD2437A1MZ are connected only via I2C.)
For reference, here are the versions I am using:
I am currently using Sigma Studio + version 2.3. I also tried version 2.2, but the result was the same.
Any advice you could offer would be highly appreciated.
Thanks,
Akinori
Please do a link first whenever you open a project.
Then, check if the "Program During Discovery" checkbox is enabled for the ADAU1452 block. This should ensure that the discovery process works correctly.
Dear arunk,
Thank you very much for your advice!
Unfortunately, even after incorporating your suggestions, the error still persists in my environment.
I would greatly appreciate it if you could provide further advice or insights if you notice anything else.
Thank you.
Thanks to the support from the distributor and the ADI professional staff, I was able to resolve the issue successfully. I would like to share the key points that helped me solve the problem, in case they are helpful to others:
I hope this information proves useful to others who may encounter similar challenges. Many thanks to the community for the helpful discussions and insights.