Post Go back to editing

Help with identifying correct A2B products in connecting 2 IVI systems

Category: Hardware
Hi All,
 
I am part of Intel Automotive Division and we would like to present to our customers a A2B use case.
Our product is a base platform for future IVI systems. We would like to show how one could connect 2 of these platforms to demonstrate the A2B use case.
A2B Diagram
The 2 devices which we want to connect via A2B, have I2S headers on which I know how to transmit Audio data on its TX and record on its RX:
I2S Header

What I need help with is with:
  1. The A2B transmitters, these can be evaluation boards.
  2. Any special cables that would connect the A2B transmitters to the main/sub device or between themselves.
  3. How to configure the 2 transmitters so when I play on the I2S header TX it will transmit the Audio signal all the way to the sub device where I can record from the I2S header RX.
Please help me identify the Analog Devices products that could help us show this A2B use case.
Also any help on how to do the SW and HW configuration would be greatly appreciated.
 
Best Regards,
Alex