Hello,
I am working with Sigma Studio with the following A2B network:
- Master node: EVAL-AD2435WA3LZ
- Slave node: ADZS-AD2435MINI connected via I2C to a class D amplifier

I would like to monitor the status of some amplifier registers, so I have added the amplifier register I would like to check to the Fields to Monitor in the Target processor monitor, with time interval of 5s.
But, I am not able to get the values of the registers, I always get a blank column, as you can see in the picture below.
Moreover, during the monitoring, I get some error on the master board (e.g., "Line fault error" or that the master board is disconnected), but I think they are not real errors, since the system is working and can play sound.
The only values I can get with the monitor are the values of the registers of the audio host, which is directly connected to the PC (target processor).
Should I be able to read also the amplifier registers with this monitor? Or are there any other methods to perform periodic reading?